STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1562 Views
  • 0 replies
  • 2 kudos

REENT compilation errors when upgrading CubeMX to 1.9.0

I upgraded my IDE to STM32IDE 1.9.0, and CubeMX to version 6.5.0 in order to develop on U5 familiy.I know the ST does not include freertos lib on CubeMX 6.5.0 any more.. but, since I allready working with it in other projects I would to keep it inste...

AA.10 by Associate III
  • 816 Views
  • 0 replies
  • 0 kudos

Externai interupts for I/O pin in OUTPUT

I'm using a board Nucleo Stm32F401RE on Stm32Cube 1.8.A simple question : I have cofigured, in MX, I/O pin PC5 as GPIO_EXT_INT5with interrupt in falling edge , pull_up enabled and NVIC[9:5] enabledRemember: in Nucleo board PA5 pin control in OUTPU...

LVara.1 by Associate II
  • 3550 Views
  • 7 replies
  • 0 kudos

ERR_MEM on lwip stack

Hello!I use MCU STM32F429ZIT6. My task is to receive data on UART for several hours and copy them to ethernet. My function to send data (I generated the code in the CubeMX program with no RTOS): void sendstring (char* buf_str) { tcp_sent (ss->pcb, tc...

DFomi.1 by Associate II
  • 3474 Views
  • 2 replies
  • 0 kudos

How to debug an USB-Connection?

Hello everyone,I am trying to expand the STM32Cube USB library which comes with the generated Code from STM32CubeMX. There are still some bugs in the Code but it is really hard to find them without appropriate debugging tools. The normal debugger can...

THe1 by Associate
  • 4751 Views
  • 4 replies
  • 0 kudos

CubeMX Forcing FreeRTOS to be included on STM32H7

This is really a CubeMX problem but didn't see a better forum to post to. I am trying to create a bare metal project with CubeMX for the STM32H7. I click File->New Project..., then select STM32H745/755 under the Line drop down on the MCU/MPU Select...

ttatakis by Associate III
  • 1725 Views
  • 1 replies
  • 1 kudos

Resolved! H743+FreeRtos+LWIP errno bug?

Hi everyone. After some updates of CubeIde I have returned to an old project and can not compile it. IDE shows me the error of multiple definitions of errno variable. I tried to start a clean project. When I enable FreeRtos and LWIP it shows me the s...

CubMX 6.5.0 ADC issue with STM32G0

Hallo,after Upgrading to CubeMX 6.5.0 there are problems using ADC1 with STM32G070RBT6. When the 'Number of Conversion' > 1 it is not possible to set 'Discontinuous Conversion Mode' to Disabled (only Enabled), with CubeMX 6.4.0 it works. Is this a bu...