STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1626 Views
  • 0 replies
  • 2 kudos

how to use external RTC

I'm using STM32G070KBT6 controller. I'm trying to use external RTC and External RTC were ( DS1341). i2c based RTC.Here is my code/* Private user code ---------------------------------------------------------*//* USER CODE BEGIN 0 */// Convert normal ...

0693W00000Lwlc2QAB.png

Resolved! STM32CubeMX and STM32F4xx still low TCP/IP transmit performance

Hi, anybody,I am using STM32F407ZG/STM32F429IG to build two similar control board. The main function issome host send amount of data, about 1M bytes (STM32F407 with FSMC/SRAM) or 32M bytes (STM32F429 with FMC/SDRAM)to STM32 and stored in memory. Then...

PZhan.11 by Associate II
  • 2482 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L151C8T6A clock configuration in CubeMX

The Clock Configuration tab in CubeMX is not happy and I cannot figure out what the problem is exactly. I only want to use HSE a 25MHz external clock source in BYPASS. And I do not intend to use the PLL. Is this a bug in the tool? How can I satisfy t...

0693W00000LweunQAB.png

Need help to use SD card device on STM32H753I-EVAL2.

Hello,We just purchased the STM32H753I-EVAL2 board and have a problem with initializing the SD card device.With CubeMX, we create a default project:- new project/board selector/STM32H753I-EVAL2- "Initialize all devices with their Default Mode" --> Ye...

WWant.1 by Associate II
  • 2739 Views
  • 4 replies
  • 0 kudos

Resolved! STM32Cube tools and log4j

The impact of log4j vulnerabilities CVE-2021-44228 and CVE-2021-45046 for STM32Cube tools has been assessed by the development team, and the tools can be used without risk.STM32CubeMX,STM32CubeIDE,ST-MCU-FINDER-PC The log4j version used is not impact...

USART2 of STM32 Nucleo-L053R8

When using USART2 of STM32 Nucleo-L053R8, if I try to use PA0 and PA1 that are not used for flow control as GPIO, a warning appears as shown in the attached picture. How to resolve this conflict?

0693W00000LwMq9QAF.png 0693W00000LwMqdQAF.png
BSalt.1 by Associate III
  • 1397 Views
  • 3 replies
  • 0 kudos