STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1574 Views
  • 0 replies
  • 2 kudos

Resolved! Having to configure each time reading the adc value

Hello I am using stm32h750vb. I want to use an interrupt to read the adc value, but in the interrupt and dam mode the adc unit does not work. In polling mode, it shows the correct value only once after the microcontroller reset and then a constant va...

WDashti by Associate
  • 4386 Views
  • 7 replies
  • 0 kudos

Resolved! Install X-CUBE-SUBG1 in STM32CUBEMX

Hello!I want to make a basic remote control with the SPSGRF-915 module, but as far as I can understand I need the X-CUBE-SUBG1 extensión software to control it.I have already downloaded the software from ST (en.x-cube-subg1_firmware) and on the STMic...

RGarc.1 by Associate
  • 1711 Views
  • 2 replies
  • 0 kudos

Resolved! STM32U585 : ADC4 configuration

With this configuration :nbr of conversion : 2scan conversion mode : EnableContinious Conversion Mode : cannot set to Enable !!!Discontinious Conversion Mode : ucannot set to Disable !!!Unless I am mistaken, I see no indication in the STM32U5 referen...

MFred.2 by Associate III
  • 1975 Views
  • 2 replies
  • 0 kudos

Resolved! Bug in clock configuration in CubeMX 6.4.0

When trying to use the "List pinout compatible MCUs" feature to move an existing CubeMX project to a different MCU I get incorrect clock calculations in the clock configuration tab.For example, starting with a project for STM32L451RETx and then using...

0693W00000KcX4MQAV.png 0693W00000KcX5FQAV.png
KORou.1 by Associate II
  • 3638 Views
  • 6 replies
  • 0 kudos

Resolved! ADC Clock Setting in ST Cube MX for STM32H742VGT

Dear all, I used STM323H742VGT in one of my cards and I would like to configure it with ST Cube MX V6.5.0. According to the reference manual ADC clock source and pre-scaler can be set using ADCx_CCR register.I would like to use asynchronous clock sou...

TA1 by Senior
  • 3714 Views
  • 4 replies
  • 0 kudos

Resolved! Bug in STM32CubeMX for H753 ADC and work-around.

I have problems porting a H743Zi2 code to a H753. When using the .ioc file editor with the ADC the option to set the ADC clock prescalar is not present for the H753. It is there for the H743. The coeersponding line in the main.c code is not present e...

HWhit.1 by Associate III
  • 1729 Views
  • 2 replies
  • 0 kudos