STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1560 Views
  • 0 replies
  • 2 kudos

Interrupt callbacks is not working, v 6.6.0

I've followed st video lab: https://www.youtube.com/watch?v=urHGtvLYctkDebugging the code, the calback (e.g. HAL_UART_RxCpltCallback) is not called (breakpoint is set). I tried with the "Register Callback" Enabled and Disabled, but none is working. ...

ksale.1 by Senior II
  • 2193 Views
  • 3 replies
  • 0 kudos

I2C conflict with timer output

hello to everyone, i am using stm32f429zi to generate a pulse for a triac . It all function without a lcd display.when i write the code to init the display(via I2C) ,,, the display works very fine but i have a problem ... the output of timer1 doesnt ...

LFerr.7 by Associate II
  • 2073 Views
  • 2 replies
  • 0 kudos

Resolved! MX6.5.0 Pinout->List Pinout Compatible MCUs never finishes

It stops at 95% on two different machines, the Windows Task Manager runs the MX task at 95-100% up until 95% and then goes to 0 "forever". Windows 10 Pro 64bit, all service packs, Intel Core2 and i7, 12GB RAM. Processors used in IOC file STM32F767BIT...

0693W00000NqsYIQAZ.jpg
GoEk by Associate III
  • 3647 Views
  • 7 replies
  • 0 kudos

Resolved! I can not trust the MX plugin to generate the right code. I cannot get the serial port to work at all with the generated code. It used to work no problem.

First the GUI is all screwed up. When I look at USART2 It gives me the choices forGPIO output level,GPIO mode, GPIO Pull-up/Pull-downMaximum output speedUser Label,it is missing Fast Mode. I click down to USART1_TX and the list is different. It hasGP...

0693W00000NsptCQAR.png 0693W00000NspvDQAR.png
KiptonM by Lead
  • 3872 Views
  • 11 replies
  • 0 kudos

Resolved! Why does ST not publish a list of known problems with STM32CubeIDE and STM32CubeMX, and possible workarounds, until they are fixed?

I have spent hours trying to find bugs, and when I report them I am told they are "known problems". And the ST employee points to a number, that is internal to ST only. Companies publish Errata sheets all the time when the chip does not work as adver...

KiptonM by Lead
  • 1557 Views
  • 2 replies
  • 0 kudos