STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1543 Views
  • 0 replies
  • 2 kudos

(1) Which STM32F2 and (2) purchased where?

(1) Please tell me if I'm on the correct track here. I have an STM32F1 design (STM32F105RCT6TR) and a STM32CubeMX .ioc file that I used for pin-out assignment in the 64-LQFP package. This morning I created a new .ioc file for an STM32F2 (more speci...

HForr.1 by Associate II
  • 6127 Views
  • 12 replies
  • 0 kudos

Resolved! CubeMX: Project generation have problem

MCU reference : STM32F429ZITxFW package name : STM32Cube FW_F4 V1.25.0MDK ARM(Keil) version : 5.30STM32CubeMX verision : 5.6.1​at that time, i want to create code but i can not. just [the code is successfully generated under ~~ .but MDK ARM V4 projec...

CMOON.1 by Associate II
  • 10335 Views
  • 15 replies
  • 1 kudos

Need 3 cost effective USB ports

Currently, my custom PCB with STM32F105RCT6TR based on STM32CubeMX software has a single usb DEVICE port connecting to a display head that must play the role of USB Host. Note I'm also using dual CAN plus 5 analog inputs.Now I need to connect TWO usb...

HForr.1 by Associate II
  • 6657 Views
  • 15 replies
  • 0 kudos

Resolved! Servo not working with STM32F767Zi

I'm trying to control a Servo motor (MG90S) using the STM32F767Zi by leveraging the TIM2 Channel 1 (PA0). The Servo requires a 50Hz frequency (20ms) signal. The APB1 bus gives TIM2 timer port 108MHz frequency. The Servo is powered through a 5V port t...

0693W00000QMbXyQAL.png
VNaid.2 by Associate
  • 2023 Views
  • 1 replies
  • 0 kudos

CMSIS RTOS optional

Why in particular has the CMSIS freertos wrapper been chosen as the only option for the cubeMX ecosystem? Has there been any consideration to add a raw FreeRTOS API option to cubeMX?For an example of what seems iffy, see osThreadNew in cmsis_os2.c w...

_EFrie by Senior
  • 1261 Views
  • 0 replies
  • 0 kudos

Project build fails after update to CubeMX 6.1.1

Probably related to gnu-tools-for-stm32.9-2020-q2-update 746 | _ptr = _REENT;   |     ^~~~~~c:\st\stm32cubeide_1.4.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-n...