Version: 2.0.1Steps to reproduce: Create empty project for NUCLEO-F767ZI, vector table in startup code will be incorrect. /******************************************************************************
*
* The STM32F767ZITx vector table. Note that ...
Does anyone know how to coax cube IDE into wanting to use ninja as the build tool with a CMake project? I’ve been away from cube IDE for a while but the allure of CMake and advanced debugging has sucked me back in again. I’m on MacOS and ninja is av...
There seems to be a bug in the clock configuration for STM32H750XBHx. D1CPRE clock should be able to go up to 480MHz, but Cube won't take anything higher than 200MHz. HCLK is affected as well, can't set it to anything higher than 100MHzAndy
Hello,I'm developing a board with the BlueNRG-M2 module. I'm also using an ST-LINK V3 with uVision to debug/program. I'm also using the VCP made available by the ST-LINK V3 for some good old fashioned printf telemetry. The VCP is connected through...
Hello all,I’m just getting started playing around with BlueNRG 1 & 2 devices. I’d like to be able to debug with an ST-LINK V3 not using uVision. I found a patched ST LINK gdbserver in the 3.2.1 DK download but it’s an old version that doesn’t seem ...
Thanks Clive! You’re the guy I hoped would find this thread. Guess I should have been a little more verbose. I’ve copied the stldr to the ExternalLoader folder in my CubeProg install folder but it never appears in the list. I’ll try moving cube prog...