STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1559 Views
  • 0 replies
  • 2 kudos

SPI transmit and receive.

Hi All.!!!I am working on STM32F103 and using its 4-wire SPI for communication with slave whose data is 32bit and addr is 16bit.What I am trying to do is to write and read slave but i could not below is the settings that I have done in STM cube MX.Mo...

jtron.1 by Associate III
  • 5912 Views
  • 4 replies
  • 0 kudos

Resolved! How to avoid HAL_Init() when using a timer other than Systick

Hello guys,First of all I want to say that I don't like and don't use HAL library. Use LL_Library instead as long as possible.Now what brings me here is that currently I am manually porting FreeRTOS to an STM32469NI MCU. This force me to use a differ...

migmel by Senior
  • 5768 Views
  • 9 replies
  • 0 kudos

My ADC reading problem with DMA

Hello, I am working with the STM32F429-DISC1 development board. I am trying to read two adc from one channel. I can't read the code that I could read in the past. The code that worked in the morning is not working now. I may have changed a little. Pl...

0693W00000UnAJuQAN.png 0693W00000UnAJpQAN.png 0693W00000UnAJkQAN.png 0693W00000UnAJaQAN.png
MŞent.1 by Associate II
  • 2759 Views
  • 5 replies
  • 1 kudos

Resolved! CubeMX Alternate Pins not showing

HiJust updated in my PC STMCubeMx and STMCubeIDE for last version, and at this moment the functionality "Ctrl + Click" on a pin to see possible alternate pins is no longer working.This started to happen after updating CubeMX to v6.1.1 (previous versi...

STM32H745 SAI DMA Error

hello, i'm using stm32h745 mcu. i want to using SAI interface to use MEMS MIC, ADAU7002 .this sensor transmit 20bit PCM , 22050 hz data.i used CUBEMX and SAI & DMA setting is here.  i can't select SAI interface data size 20bit, so i fixed HAL Driver ...

0693W00000SvTPzQAN.png 0693W00000SvTQYQA3.jpg 0693W00000SvTPpQAN.jpg 0693W00000SvTWlQAN.png
hkim.5 by Associate
  • 1793 Views
  • 2 replies
  • 0 kudos

BUG: CubeMX-generated code fails to compile...

I regenerated files with latest CubeMX and the generated code fails to compile. Regeneration was done to incorporate a few settings changes and the latest pack for this processor; previously code generated was OK. Errors below, and I've attached the ...

Resolved! about STM32CubeMx

This morning, I installed cubemx and created a project for STM32F767IGT6 using J-link v2 to download the hex file to the board, but it didn't work. The project have included the LTDC, but I cannot get any signal(DCLK/VSYNC/HSYNC) from the test pads o...

JChen.37 by Associate II
  • 3261 Views
  • 5 replies
  • 0 kudos