Skip to main content
Lzhou.1
Associate
February 7, 2022
Solved

MX_GPIO_Init() is generated but not called in main(). STM32CubeMX6.4.0 with STM32H755XI

  • February 7, 2022
  • 2 replies
  • 2491 views

Environment:

tool: STM32CubeMX6.4.0 

cpu: STM32H755XI

Repos: STM32Cube_FW_H7_V1.9.1

I configured pins as GPIO input/output by STM32CubeMX GUI. MAX_GPIO_Init() is auto-generated and all pins are configured inside. However it is not called by any function. Usually it will be called in main().

Below is the auto-gernerated main() function code. MAX_GPIO_Init() is missed. Is it a abnormal case?

My ioc file for this case is also attached.

Thanks.

int main(void)

{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

/* USER CODE BEGIN Boot_Mode_Sequence_0 */

 int32_t timeout;

/* USER CODE END Boot_Mode_Sequence_0 */

 /* Enable I-Cache---------------------------------------------------------*/

 SCB_EnableICache();

 /* Enable D-Cache---------------------------------------------------------*/

 SCB_EnableDCache();

/* USER CODE BEGIN Boot_Mode_Sequence_1 */

 /* Wait until CPU2 boots and enters in stop mode or timeout*/

 timeout = 0xFFFF;

 while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) != RESET) && (timeout-- > 0));

 if ( timeout < 0 )

 {

 Error_Handler();

 }

/* USER CODE END Boot_Mode_Sequence_1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */

 SystemClock_Config();

/* USER CODE BEGIN Boot_Mode_Sequence_2 */

/* When system initialization is finished, Cortex-M7 will release Cortex-M4 by means of

HSEM notification */

/*HW semaphore Clock enable*/

__HAL_RCC_HSEM_CLK_ENABLE();

/*Take HSEM */

HAL_HSEM_FastTake(HSEM_ID_0);

/*Release HSEM in order to notify the CPU2(CM4)*/

HAL_HSEM_Release(HSEM_ID_0,0);

/* wait until CPU2 wakes up from stop mode */

timeout = 0xFFFF;

while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) == RESET) && (timeout-- > 0));

if ( timeout < 0 )

{

Error_Handler();

}

/* USER CODE END Boot_Mode_Sequence_2 */

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */

 MX_DMA_Init();

 MX_UART7_Init();

 MX_RTC_Init();

 MX_MDMA_Init();

 MX_QUADSPI_Init();

 MX_I2C2_Init();

 MX_SDMMC1_MMC_Init();

 MX_TIM5_Init();

 MX_UART8_Init();

 MX_DAC1_Init();

 MX_SAI1_Init();

 MX_SPI4_Init();

 MX_SPI5_Init();

 MX_UART4_Init();

 MX_RNG_Init();

 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Init scheduler */

 osKernelInitialize(); /* Call init function for freertos objects (in freertos.c) */

 MX_FREERTOS_Init();

 /* Start scheduler */

 osKernelStart();

 /* We should never get here as control is now taken by the scheduler */

 /* Infinite loop */

 /* USER CODE BEGIN WHILE */

 while (1)

 {

  /* USER CODE END WHILE */

  /* USER CODE BEGIN 3 */

 }

 /* USER CODE END 3 */

}

This topic has been closed for replies.
Best answer by Sara BEN HADJ YAHYA

Hello @Lzhou.1​ ,

Thanks for your feedback,

It seems that you checked the " Do not Generate Function Call " in your CubeMX configuration.

Could you please uncheck it and check the visibility field instead, just like the attachment below.

0693W00000JOyNOQA1.pngI hope this helps :) !

If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly :)

Sara.

2 replies

Sara BEN HADJ YAHYA
ST Technical Moderator
February 8, 2022

Hello @Lzhou.1​ ,

Thanks for your feedback,

It seems that you checked the " Do not Generate Function Call " in your CubeMX configuration.

Could you please uncheck it and check the visibility field instead, just like the attachment below.

0693W00000JOyNOQA1.pngI hope this helps :) !

If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly :)

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Lzhou.1
Lzhou.1Author
Associate
February 9, 2022

Yes, it works, thank you very much!