STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1564 Views
  • 0 replies
  • 2 kudos

Resolved! HAL vs. CMSIS layer in STM32CubeIDE (CubeMX)

Hi,I'm wondering whether I'm always getting into the HAL layer when configuring a project using the CubeMX configurator in STM32CubeIDE? Is it configurable? How to I get rid of the HAL layer while still being able to use the configurator? Where is th...

CubeIDE compatibility issues

When I use CubeMX in CubeIDE, the drop-down box for selecting a chip always closes automatically before I click. When I edit ioc files in CubeIDE, the chip area and the middle function selection area often flash. Especially in the Software Packs Comp...

0693W00000aJPSSQA4.png
AKevi.1 by Associate
  • 929 Views
  • 0 replies
  • 0 kudos

Resolved! Error during migration of project (.ioc) from STM32CubeMX V6.5.0 to STM32CubeMX V6.8.0 (STM32Cube FW_F3 V1.11.4 used)

When I try to migrate project (.ioc) from STM32CubeMX V6.5.0 to STM32CubeMX V6.8.0 (STM32Cube FW_F3 V1.11.4 used) the following hint pops up:After selection of 'Migrate' or 'Continue' the following error pops up:My question:Is there a way to migrate ...

0693W00000aJOxOQAW.jpg 0693W00000aJOxnQAG.jpg
KWoll.2 by Associate II
  • 1829 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeMX 6.8 Changes VOS on STM32H745 again

I'm building several projects based on STM32H745 and upgraded to STM32CubeMX 6.8. Upon doing so, VOS0 no longer is an option when using PWR_DIRECT_SMPS_SUPPLY:6.7: Now with 6.8: Of course, this changes all the peripheral speeds and causes many proble...

0693W00000aJHdgQAG.png 0693W00000aJHdqQAG.png

Resolved! SPI transmit with interrupt not work

Hello to everybody,I have program for stm32f103 mcu. Now I want to do my SPI transmit routine using interrupt.Before:HAL_StatusTypeDef status = HAL_SPI_Transmit(&afe_spi, (uint8_t*) pData, 4,100);Now I tried this (and many variants also):HAL_StatusTy...

0693W00000aJKXCQA4.png 0693W00000aJKXWQA4.png 0693W00000aJKXqQAO.png
EBurk.1 by Associate II
  • 3933 Views
  • 7 replies
  • 0 kudos

STM32G4A1KEU6 - FreeRTOS - CubeMX Break at address "0x1fff4cf8" with no debug information available, or outside of program code.

When generating a blank project for a STM32G4A1KEU6 I'm able to debug the code.As soon as FreeRTOS is added (USE_NEWLIB_REENTRANT activated, Time base source is TIM6, Debug is Serial Wire) and no other peripherals are activated, I'm not able anymore ...

Resolved! Switch from stm32f407 to stm32h753

Hi,I want to switch a project in cubemx from stm32f407 to the stm32h753. (both lqfp100in cubeMX 6.8.0 there is this pinout feature to show compatible cpus. cubeMX lists me all the variants of the stm32F4, L4 and F7 but there are no H7 listed.Is there...

Jnevi.1 by Senior
  • 4374 Views
  • 5 replies
  • 0 kudos

Resolved! When will STM32CubeMX will be up to date concerning FreeRTOS?

Hello,I'm working with:STM32CubeMX version 6.8 (last version)STM32F4 FW version 1.27.1 (last version again)And, when generating a project with FreeRTOS, the FreeRTOS version is 10.3.1This version has been released more than 3 years ago!! It is comple...

ANauz.1 by Senior II
  • 1815 Views
  • 1 replies
  • 0 kudos