User Activity

USB Host Driver for MSC does not work.After upgrading one of my programs to the latest version of the Cube-HAL, my program with USB Host (USB FS) MSC on a STM32F746-Nucleo board stopped working. I use RTOS. The program still recognizes the device and...
Processor STM32F746ZGTHello,When I use FreeRTOS (CMSIS_V2) in STM32CubeIDE 1.9.0, I get the prompt when generating code (as in the previous versions):The USE_NEWLIB_REENTRANT must be set in order to make sure that newlib is fully reentrant. The opti...
I have tried to download the Windows version of STM32CubeIDE 1.7.0. The file size of the zip file is about 70 MByte. The file is not a valid zip file. 
STM32F746 V1.14 CubeMX 5.0.1 and V1.15 5.103 ranks definedmissing statementssConfigInjected.InjectedRank = ADC_INJECTED_RANK_2;sConfigInjected.InjectedRank = ADC_INJECTED_RANK_3;in generated code
Posted on March 21, 2018 at 09:00I have tried to use SWV on DISCO-Board STM32F746 with Firmware V2J30M19. It does not work. But it works with Firmware V2J29M18.On Nucleo STM32F746 SWV work with both Firmware versions.Is this a common problem?
Kudos from