STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

Problem with USB_Host_Library

Have STM32H7B3 Discovery Kit.Used CubeMX to create IAR project.Integrated USB_Host_Library.Have USB mouse connected to OTG HS port.Find that USB initialization eventually triggers a configASSERT(pxUnblockedTCB) in source tasks.c function xTaskRemoveF...

Stuck in HOST_DEV_WAIT_FOR_ATTACHMENT while usb

Hi.. I am working with stm32f429disco 1.. .I have generated with cube mx the fw init for usb host.. When I start my fw with the usb stick connected at least I am able to go inside the routine USBH_Process but when i run again the fw i am not able to ...

_legacyfs_online_stmicro_images_0693W00000dJptRQAS.png
SGasp.1 by Senior
  • 3131 Views
  • 6 replies
  • 1 kudos

Making a pulse counter with LPTIM4

I'm trying to use the LPTIM4 while in STOPMode2, in a stm32U575ZI-Q microcontroller, as a external pulse counter, and use this pulse value to refresh a LCD screen. For this question I'm only using the usart1 to tell me how many pulses were detected i...

Resolved! How to install STM32Cube_FW_F4_V1.27.0

Hi,I have just installed STM32CubeIDE Version: 1.12.1 Build: 16088_20230420_1057 (UTC) onto my Kubuntu 22.04.2 LTS (fully updated) system. The install process ended stating that the IDE had been installed correctly.I then wanted to install the packag...

Target Software Startup Script Error

Hello All,I am using STM32F777IITx MCU based custom board with STM32CubeMx v4.24.I want to built a application where i want to Read/Write data from/to flash.I am have written a small application where i write 10 bytes of data to flash and also read t...

0690X00000ApQKYQA3.png

IWDG and handling of window option during HAL_IWDG_Init.

HAL_IWDG_Init is implemented in file stm32L4xx_hal. Here two statement from the L476 documentation: a) "When the independent watchdog is started by writing the value 0x0000 CCCC in the IWDG key register (IWDG_KR), the counter starts counting down fro...

MJord by Associate
  • 5298 Views
  • 1 replies
  • 0 kudos

SPI3 Clock not working on NucleoU575

Hello all, I want to use a NucleoU575 board to test an accelerometer sensor.I have written the driver for this accelerometer and currently, without having it connected to the Nucleo, I am trying to check whether my SPI3 Clock is working.This is the c...

_legacyfs_online_stmicro_images_0693W00000dDPOjQAO.png
KKots.1 by Associate II
  • 1942 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H745II VOS with SMPS supplying LDO

Greetings,What is the reason for not being able to use the SMPS (or the SMPS supplying LDO) option for VOS0 on STM32H745II?VOS0 means the highest voltage, so won't the dissipation on the LDO be the highest?I have been using the PWR_SMPS_1V8_SUPPLIES_...

DTomi.1 by Senior
  • 10623 Views
  • 21 replies
  • 4 kudos

No interrupt in SDcard with DMA on STM32L476 and CubeMX

Hi, I have an unsolved issue with SDcard.The project is based on STM32L476, the IDE is Atollic and configuration is made by STM32CucbeMX (as I do with all my designs).Without DMA (no DMA template in FATFS and no configured DMA channels) the SDcard wo...

0693W00000D0ny7QAB.png 0693W00000D0ntHQAR.png
MarcoM by Associate II
  • 4695 Views
  • 9 replies
  • 0 kudos

HAL_HCD_Disconnect_Callback called usb host stm32f429disco 1

Hi community.. I am working with stm32f429disco1 (the one with display) I created the code with cube mx and you can find it here in the attachments.. The usb host function it is not working.. I am able to get just at the beginning one connection phos...

SGasp.1 by Senior
  • 3386 Views
  • 8 replies
  • 0 kudos