User Activity

This is not a bug of the forum engine, but of the main ST web server! Let's open the following link:https://www.st.com/resource/en/application_note/an2606-stm32-microcontroller-system-memory-boot-mode-stmicroelectronics.pdfBy default on a Chromium/Bl...
If one takes a link to a specific post, then the posts, which had been moved from other topics, show the title of their respective original topic.Original post (OK)Moved post (wrong title):Also, as I have reported previously, adding a "Re: " in front...
Dragged a mouse accidentally over this post down there. Pressed at least one or both of the left/right mouse buttons at the same time. The screenshot has not been modified...The only interaction with the page, that still works:Scrolling. Also middle ...
UM1974 Rev 10, Table 1. Ordering information:For the NUCLEO-F303ZE board the column "Differentiating features" lists an "Ethernet", which is false.Of course a deceptive photo and description just adds to the confusion...https://www.st.com/en/evaluati...
Every day some alternatively gifted user creates a duplicate topics, people often comment on more than one of those and in the end the information is scattered in around and is a mess. For an example:https://community.st.com/t5/stm32-mcus-embedded-so...