STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1681 Views
  • 0 replies
  • 2 kudos

Resolved! Bug: STM32CubeMX 6.8.1 STM32G431 TIM1 LL init code generation

how to reproduce:generate a new C project for Nucleo-G431RB with all default settings.enable TIM1 with internal clock sourceset the prescaler to 170-1set code generation for TIM to LLgenerated code:   /* USER CODE END TIM1_Init 1 */ TIM_InitStruct...

KnarfB by Super User
  • 2507 Views
  • 1 replies
  • 0 kudos

H743 and LAN8742 init

I'm still struggling with the ethernet code. I have some custom hardware that where several H743 controllers are powered on at the same time and sometimes they don't get all a connection (no IP address from dhcp). But I can reproduce this error as we...

JojoS by Associate III
  • 7103 Views
  • 8 replies
  • 3 kudos

USE_NEWLIB_REENTRANT

After enabling USE_NEWLIB_REENTRANT in FREERTOS (pic.1) I get error notification in LWIP (pic.2) and also after I try to compile this settings (pic3). This error info disappear when I manually put in 1 in the fieldwith red error text (pic.2 > RTOS De...

1.jpg 2.jpg 3.jpg
MCUpwr by Associate III
  • 1946 Views
  • 0 replies
  • 0 kudos

CubeMX 6.8.1 for F7 does not support FreeRTOS 10.3.1

I'm porting an active application project from F4 to F7 (The customer had to change as of the problem to get F4 MCUs).The current project that was generated with CubeMX used FreeRTOS 10.3.1 as this is the version that the CubeMX support.Now, when I p...

Egolt.1 by Associate III
  • 1223 Views
  • 0 replies
  • 0 kudos

STM32Cube FW_L1 V1.10.3 library has a bug and does not support ADC regular group conversions greater than 16 (conversions) ranks.

The CubeMX correctly allows selection of up to 28 conversions, but generated code fails when set above 16. The libraries sequencer scan length definitions end at LL_ADC_REG_SEQ_SCAN_ENABLE_16RANKS and ADC_SQR1_L_4 is not found in the libraries but ex...

robd by Associate II
  • 2219 Views
  • 2 replies
  • 0 kudos

I2C EEPROM TO WRITE AD DATA USING STM32F103C8T6 MCU

Hello,    I am try to write the data for memory address in EEPROM using standard protocol I2C. we are trying in data write to memory Address and Driver IC read to operates the Sensorless BLDC motor. so I am working in this method. But am put in the d...

Screenshot (63).png 42544sg.PNG
mrsmile by Associate III
  • 3417 Views
  • 2 replies
  • 0 kudos

H743ZI + lwIP DHCP problem

I have a project with STM32H743ZI, lwIP, noOS. I've read the document with the suggested settings for MPU, linker file, lwIP head placement and applied the changes to CubeMX generated code.Additionally, I have set the MEM_ALIGNMENT to 32 bytes and ad...

JojoS_0-1687093051524.png
JojoS by Associate III
  • 2651 Views
  • 2 replies
  • 2 kudos

unit testing in cube ide as of 2023

HiI need to do some unit testing. As of 2023 What is the easiest way forward? Which tool is best integrated with CUBE ide?There are 2 use cases:Unit tests running on STM32 (here I just know of Tessy/Hitex, not open source)?unit tests running on a win...

MK..1 by Senior
  • 1495 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.