STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

Resolved! MX_SDIO_SD_Init wrong bus wide initialization

I have a STM32F407 with an SD card wired in 4-bytes mode and FATFS middleware to manage the files.I upgraded to STM32CubeIDE 1.11 two weeks ago, but since then the SD card stopped working. The initialization fails in the SD_WideBus_Enable function, s...

FRugi.1 by Associate
  • 4981 Views
  • 3 replies
  • 1 kudos

Algobuild software package not downloading in CubeMX for Mac

Trying to download Algobuild for CubeMx for Mac. The software package selector says it needs to be downloaded. There is a yellow triangle with an exclamation next to the word "Download". Clicking it does nothing and no explanation what the yellow tri...

Davidcs by Associate
  • 2197 Views
  • 3 replies
  • 0 kudos

STM32CubeMX 6.9.0 released

We are pleased to announce you that the official release of STM32CubeMX V6.9.0 is available for download here What is new in STM32CubeMX V6.9.0? Added the support for new microcontrollers in the STM32U5 seriesAdded the support for new microcontroller...

Resolved! CubeMX feature request: Pinout view for nucleo boards

It would be very useful and I think relative easy to implement: To have an alternative pinout view but instead of the the IC, a view of the nucleo board with the morpho and arduino connectors.Something like this but interactive: https://os.mbed.com/p...

DAlvarez by Associate II
  • 1694 Views
  • 1 replies
  • 2 kudos

NOT A VALID .IOC FILE

Hi,I have got a problem here with stm32cubemx whenever i select generate code  i will get a dialogue box as not a valid .ioc filecould you please provide solution for this

Resolved! Configure location of STM32CubeMX generated code

This seems like an easy one, but I've searched high and low.  Both STM32CubeMX (v6.9.2)  and STM32CubeIDE (v1.13.2) place generated code in a root folder named Core.  Is there a way to configure file placement into folders of my choice?

BillyBob by Associate II
  • 1998 Views
  • 1 replies
  • 0 kudos

CDC_Transmit_FS function always returns USBD_BUSY

I am now trying to implement CDC-VCP connection between a PC and a STM32 board. Just my goal is a STM32 echo server.​I have done like this: ​STM32 Cube MX : USB FS endableUSB Device : CDC Enable, rx/tx buffer size as 128<-1000Clock config : USB 48MHz...

SSON.2 by Associate II
  • 10127 Views
  • 5 replies
  • 0 kudos

Resolved! STM32CUBEMX 不自动生成代码问题

第一次在论坛中请教问题,如果有不对的地方,请及时通知修改,感谢 我在使用STM32H750XBH6 ,在使用STM32CUBEMX 自动生成代码时出现了问题,DMA的初始化代码没有自动生成,在不停地测试中发现,DMA Request 选择 dma_generator0-dma_generator7、MEM2MEM , 可以生成代码,选择定时比较捕获输出通道作为请求源没有自动生成代码(例如 tim4_ch1\ch2 ,tim3_ch3\ch4),cubemx版本号6.92,希望可以得到一些解决的建...

mingmieg by Associate II
  • 3932 Views
  • 2 replies
  • 0 kudos