STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

issue after migrating to new version STM CUBE MX

Hi everybody I have errors in code mainly in RTOS file and TASK file after Updating the new STM32 CUBE MX generating code any one have any idea about these things  note :My code is working fine with old version of STM cube Mx i am using IAR workbench...

PESHWA by Associate II
  • 1179 Views
  • 1 replies
  • 0 kudos

Resolved! CubeMX generated code doesn't work when mixing use HAL and LL

My project running on STM32G071 uses LL drivers for ADC and USART. The configuration code is generated by STM32CubeMX.  It works fine. However after adding I2C HAL module which connects to a sensor to the project, the I2C function HAL_I2C_IsDeviceRea...

why_q_0-1696428687162.png why_q_1-1696429012212.png
why_q by Associate II
  • 2953 Views
  • 5 replies
  • 2 kudos

IAP with Ymodem has an error when first send the file.

Like subject when I powered on my mcu board and sent '.bin' file first, it occured an error "The image size is higher than the allowed space memory".But Sent same '.bin' file again, it's OK.I used to STM32F429ZI, IAR Compiler and  Menu.c & .h , commo...

UTU by Associate
  • 1382 Views
  • 1 replies
  • 0 kudos

Resolved! Cube MX custom template for custom folder structure

The STM32CubeMX User Manual (UM1718 section 3) and various threads on this forum lead me to believe I can customize the folder structure that CubeMX uses for where it puts the code files it generates. I'm not trying to do anything fancy, I'd just lik...

magene by Senior II
  • 2862 Views
  • 1 replies
  • 0 kudos

Non-secure interrupts are not working with trustzone enabled

CubeMX generates a file called "partition_stm32h563xx.h", this file contains the settings of which interrupts are available in the non-secure area, when trustzone is enabled.For stm32h563 the generated list of interrupts is wrong.There are many inter...

Mogens by Associate
  • 1271 Views
  • 1 replies
  • 0 kudos

Resolved! Generated HAL Timer Tick generated code has an error - F7

I am using STM32CubeIDE 1.13.2 with STM32CubeMX 6.9.2-RC4.  It is an STM32F746 processor.  I'm using STM32Cube_FW_F7_V1.17.1 libraries.  I'm using Azure RTOS and selected TIM12 for the HAL tick time base.This is a side issue.  When TIM12 was selected...

tec683 by Associate III
  • 2779 Views
  • 1 replies
  • 0 kudos