STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1588 Views
  • 0 replies
  • 2 kudos

Is it possible to add custom USER CODE sections?

We are using the ST MCSDK, it is very helpful. In MCSDK/MCLib/Any/Src there is a function called STM_FaultProcessing. It is auto generated by Cube. We have one line we want to add to it that turns an LED on alerting the user to a problem. This wo...

0690X000006DfARQA0.png
MRyan.7 by Associate III
  • 8455 Views
  • 3 replies
  • 9 kudos

Resolved! STM32U5A5 : GPMDA Linked List, what is Datasize

pNodeConfig.SrcAddress = &(ADC1->DR); pNodeConfig.DstAddress = (uint32_t) adc_values_1; pNodeConfig.DataSize = 4*64;In reference to the above based on an excellent tutorial (STM32U5 Workshop) which I use for nucleo STM32U5A5 https://www.youtube...

Riscy by Senior
  • 2182 Views
  • 2 replies
  • 1 kudos

Resolved! Detection of repository version in an existing project

Hello!I have created a project using cubemx a few years ago. i know which cubemx version i have used in this project but i cant seem to find out which cube repository version i have used.  What is the way to find it? can i find the repository version...

yuri CH by Senior
  • 3203 Views
  • 5 replies
  • 0 kudos

Resolved! CubeMX version error

I'm using STM32CubeIDE 1.11 and I want to import an existing file:File --> Import --> Exsisting Projects into Workspace --> Select Root DirectoryI get the following error when I try to open the .ioc file:File --> Import --> Exsisting Projects into Wo...

luke514_0-1701338365709.png luke514_0-1701339352262.png
luke514 by Senior
  • 2272 Views
  • 3 replies
  • 1 kudos

Resolved! STM32CudeMX base code generates a larger program file

Hi I made a program for STM32F103RG using STM32CubeMX and STM32CubeIDE a few years ago. The program is using the USB Device Mass storage software pack. I thought that I should update it with the latest version of it and made a new project since the o...

Resolved! STM32F746: ADC3 does not work with external trigger from timer

Hi,I made project that samples audio signals from the ADC at a constant rate. The trigger signal for the ADC conversion is generated by a timer. Now here's the thing:The code works fine on my STM32L432 Nucleo, STM32L4R5 Nucleo and STM32F429 Disco, bu...

SFahr by Associate III
  • 4744 Views
  • 8 replies
  • 0 kudos