cancel
Showing results for 
Search instead for 
Did you mean: 

How to select STM32H743 lwip's system timebase source?

span.1
Associate

Good day sir.

ST's EVM�?development software and firmware informations or else are as ​below :

  • NUCLEO-H743ZI2​
  • CubeMX : 6.2.1
  • CubeIDE : 1.1.0.1​
  • Firmware package : STM32Cube FW_H7 V1.9.0
  • lwip : 2.1.2, raw api without rtos.

After modifying according to the How-to-create-project-for-STM32H7-with-Ethernet-and-LwIP-stack-working setting, currently PC PING to the EVM board�?EVM board as the TCP/UDP client that working fine. EVM board as the TCP/UDP server, after running for a while, PC can't ping the EVM board what a problem with the lwip parameter setting I guess, however that's not my point.

Currently SYS time source of test project is TIM6(1mS measurement from oscilloscope), what If I set the SYS time source to SysTick or else. are there any issues/problem problem occurred when lwip working?​

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Piranha
Chief II

Update your software! Before CubeH7 v1.10 the Ethernet was basically dysfunctional.

https://community.st.com/s/question/0D50X0000BOtfhnSQB/how-to-make-ethernet-and-lwip-working-on-stm32

Without RTOS the SysTick is the best and default choice.

span.1
Associate

good day sir

Currently version of the software ,CubeMX :6.5.0, STM32Cube FW_H7 V1.10.0.

lwip 2.1.2 rawapi withour rtos.

Have any example?