Skip to main content
Associate
February 8, 2024
Question

RCC frequency differences between MX generated code and standard library code at 48Hz

  • February 8, 2024
  • 2 replies
  • 1539 views

Working in the MX and with a PicoScope, I measured some square waves looking to see how the MX generated code compared to the standard library code in loop time. I was changing frequency using the 8Hz HSI through the PLL multiplier.  I found that with the MX generate code:

HAL_GPIO_TogglePin(LED_1_GPIO_Port, LED_1_Pin);
HAL_GPIO_WritePin(LED_1_GPIO_Port, LED_1_Pin, GPIO_PIN_RESET);
HAL_GPIO_WritePin(LED_1_GPIO_Port, LED_1_Pin, GPIO_PIN_SET);

The toggle at 48Hz was slower(2.5micro seconds) than at 32 Hz(1.9micro seconds). WritePin was also slower: 48Hz at 2.3 microseconds, to 1.7 microseconds at 32Hz

 

Using this standard library code, 48Hz was faster than 32Hz, as expected:


DigWrite_GPIOC(4, 1);
DigWrite_GPIOC(4, 0);

(3.9microseconds at 48Hz, and 2.2 microseconds at 32Hz)


GPIOC->BSRR = 0x0010;
GPIOC->BRR = 0x0010;

(392ns at 48Hz, 332ns at 32Hz)

 

This was all done in the MX through the PLL at 8Hz by 6 divided by 1 for 48Hz, and 8Hz by 4 divided by 1 for 32 Hz.

The standard library functions were used in the HAL generated code body, as were the HAL generated functions. 

Has anyone else has experienced this?

Thanks!

This topic has been closed for replies.

2 replies

ittyBittyAuthor
Associate
February 8, 2024

Sorry.....MHz, not Hz.

TDK
February 8, 2024

What chip? HSI has a /2 divisor on at least some F0 chips, didn't see that mentioned.

Weird. It should scale with clock speed. Did you verify clock settings using MCO out or something else?

> GPIOC->BRR = 0x0010;

This isn't a valid statement. Makes me wonder how you're compiling.

> Sorry.....MHz, not Hz.

You can edit your post. Click the down arrow at the top-right of your post.

"If you feel a post has answered your question, please click ""Accept as Solution""."