I migrated a project from STM32CubeMX 6.3.0 to STM32CubeMX 6.10.0. It didn't boot anymore.There was this interesting diff to the linker script: ** Abstract : Linker script for STM32L452VCIx series
-** 256Kbytes FLASH and 160Kbytes...
There is this in the datasheet, the SRAM2 region has two mappings:• 32 Kbyte located at address 0x1000 0000 with hardware parity check (SRAM2).This memory is also mapped at address 0x2002 0000, offering a contiguous addressspace with the SRAM1 (32 K...