Resolved! how works the CSS clock detection when he is enable?
Hi,We had enable the Clock secure system in out project.How works this?When the source clock fails what we must doing in the call-back HAL_RCC_CSSCallback()?regards
Hi,We had enable the Clock secure system in out project.How works this?When the source clock fails what we must doing in the call-back HAL_RCC_CSSCallback()?regards
Hello, I've got problem with STMCubeIDE. You can see my problem at photos I attached. Can anyone help me to solve this problem. I try to work on Lenovo Legion 5 with Ryzen 5 5600h and RTX3060. Second graphic card is integrated with Ryzen CPU. This pr...
My project running on STM32G071 uses LL drivers for ADC and USART. The configuration code is generated by STM32CubeMX. It works fine. However after adding I2C HAL module which connects to a sensor to the project, the I2C function HAL_I2C_IsDeviceRea...
I'm creating a new project for STM32G030F6P6 in STM32CubeMX. It says 32 kBytes flash. But when I look at the generated project in the file stm32g030xx_flash.icf it says: /*###ICF### Section handled by ICF editor, don't touch! ****/ /*-Editor anno...
I encountered a problem with building project from STM32CubeMX v6.9.1 with generated Makefile and CMSIS_V2 enabled. Starting build by 'make' returns an error 1 for /main.o "Can not find specified file". On the other hand, when using CMSIS_V1 everythi...
STM32CubeIDE 1.13.1 was released on st.com as well as an in-tool update patch aligned with STM32CubeMX v6.9.1 that is available for download.Main issues fixed in this patch:This patch release fixes the issues related to the following cases:STM32CubeM...
Hi, I write to report a possible bug in generating a project by selecting an STM32G0B1CB MCU.I created the basic project using STM32CubeMX (6.9.0).In the autogenerated file "stm32g0b1xx.h" (in Drivers/CMSIS/Device/ST/STM32G0xx/Include) there is the f...
I have a design with a STM32G030J6 (SOIC8) controller. I don't need an external reset. I want to use the pin 4 as a GPIO (PA1). I connect a button to this input. I select the appropriate option in CubeMX, but when the button is clicked, the controlle...
I'm looking at using the MX25L3233F for flash storage. This is a serial NOR device. It appears to support QuadSPI, but it also appears to support regular SPI:"MX25L3233F features a serial peripheral interface and software protocol allowing operatio...
Hello, I am try to write the data for memory address in EEPROM using standard protocol I2C. we are trying in data write to memory Address and Driver IC read to operates the Sensorless BLDC motor. so I am working in this method. But am put in the d...