STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1526 Views
  • 0 replies
  • 2 kudos

CubeMX & STM32G4xx & FDCAN - BUG in CubeMX

Hello,I use CubeMX V6.13.0 (now the newest version).I have find out a bug in the configuration wizzard from the FDCAN with the STM32G473.When I chose:FDCAN1, Clock Divider = "Divide kernel clock by 10"FDCAN2, Clock Divider = "Divide kernel clock by 1...

MMüll.6 by Associate III
  • 2429 Views
  • 6 replies
  • 0 kudos

CubeMX Custom Queue Sizes in FreeRTOS

I am having trouble creating custom queue sizes and making them work with the Heap Usage tool within CubeMX.  But I found a workaround until the bug gets fixed.I created a queue using a custom item size (the message_data_t type is defined in my code)...

eweststrate_0-1738710049448.png eweststrate_1-1738710182293.png eweststrate_2-1738710291653.png

Resolved! STM32 CUBEMX not starting

Hi developers.I have the same issue as many others, which has been posted already 4-5 times and marked as "solved" in some of them, but it is not at all the case.The CubeMX on launsching shows the first screen (splash) and then disappears.It worked a...

kova by Associate II
  • 4957 Views
  • 8 replies
  • 7 kudos

2 bugs with VREFBUF and STM32Cube on at least STM32G491

Hi ST,There are 2 bugs in Initialization of VREFBUF.in STM32CubeIDE V1.11.0.I use FreeRTOS, but it shouldn't have any inffluence on these bugs.1.) At function main, the firsr call is to Hal Init and when VREFBuF ist activated, in function HAL_MspInit...

Osto by Senior
  • 4071 Views
  • 5 replies
  • 1 kudos