STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1578 Views
  • 0 replies
  • 2 kudos

STM32CubeMX 4.18.0 - bug, deleted startup_stm32fxxxxx.s

Posted on November 27, 2016 at 02:16I tried the new version of STM32CubeMX 4.18.0. If I generate project for MDK-ARM V5 will be deleted the startup_stm32fxxxxx.s file in the path Drivers/CMSIS/Device/ST/STM32Fxxx/Source/Templates/gcc. Similarly, if...

CubeMX 4.18.0 compatible processor conversion bug

Posted on November 28, 2016 at 23:27I converted my project from using a '407VGT6 to using a '405VGT6 (very painless), BUT I lost all of my DMA settings and all of my interrupt priorities.Version control is my friend.Andrei from The Great White North...

STM32 Nucleo L476 Internal Temperature Sensor

Posted on July 20, 2016 at 23:00Hello,I'm trying to get the internal temperature sensor to work. But the whole time, the sampled values are too low. If I use that fancy formula from the reference guide, it says there are about 10�C, but believe me, ...

STM32L4 without Crystal for CAN, I2C and SPI

Posted on November 15, 2016 at 11:00Hello everyone,I am planing a few Sensors and remote switches which communicate using the CAN Bus. I'd like to use the STM32L433CC MCU because of its easy solderability by hand for prototyping. The boards should b...

STM32CubeFx Examples generated by STM32CubeMX

Posted on February 26, 2016 at 10:34Hi CubeMX team, why are not firmware examples for development boards written using STM32CubeMX ? I think it would help to quickly find errors in STM32CubeMX. Also, customers should share original ioc file for dev...

CubeMx 4.17 does not handle -q or -s switch

Posted on November 28, 2016 at 15:38 Hi, I recently discovered in UM1718 that CubeMX can work with a command line. That's a cool feature for continuous integration. But it seems that the command line switch are not handled. If I use ...

JulienD by Senior
  • 3053 Views
  • 7 replies
  • 0 kudos

Bug, Code generation in STM32CubeMX

Posted on September 26, 2016 at 07:16Hello,I used STM32CubeMX with 4.16.0 or 4.16.1 version.below situation :''STM32Cube Firmware Library Package'' option is ''Add necessary library files as reference in the toolchain project configuration file''IAR...

0690X00000604maQAA.png

STM32CubeMX - BUG REPORT - F411VETx Temperature sensor Channel

Posted on October 31, 2016 at 13:29Hello!After migrating to version 4.17 I have encountered problem with temperature sensor channel. I am working with it on a daily basis and I've never had any problems with it before.Problem:When i open fresh proje...

0690X00000604msQAA.png 0690X00000604w8QAA.png
bartek by Associate
  • 2245 Views
  • 4 replies
  • 0 kudos

STM32CubeMX suggestion

Posted on November 25, 2016 at 12:45Would be good to avoid generation of peripherals initialization code if using CMSIS Driver.CMSIS Driver does complete initialization of the related peripheral. So, the code, generated by STM32CubeMX is not used.I ...

Eugene S. by Associate III
  • 884 Views
  • 1 replies
  • 0 kudos