User Activity

Hello, I designed a similar board using STM32H743ZIT6 and STM32H743VIT6. (Rev. V)The board works fine normally.It has been in production for 3 years already. Boards that have already been produced and shipped sometimes become unusable. (since a few m...
 I make a new product with NetXDuo for STM32H743.But, it is included error code in RTE_Components.h RTE_Components.h (A project)/* USER CODE END Header */ /* Define to prevent recursive inclusion -------------------------------------*/ #ifndef __R...
Hello,First of all, NetXDuo is working fine on the NUCLEO-H743ZI board. (PING, UDP, TCP) Environment :STM32CubeIDE v1.17.0STM32CubeMX v6.13.0STM32Cube_H7(HAL) v1.12.1X-CUBE-AZRTOS-H7 v3.3.0 I modified it to fit my custom board.The clock for the PHY c...
안녕하십니까?STM32H743�?� 예로 들 경우,​MEMORY{RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512KRAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288KRAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K}​​와 같�?� �?역�?� 있�?� 때, RAM_D1�?� 공간�?� 부족하여​.data 섹션�? 대해서 RAM_D1과...
Hello,I want to generation code with FreeRTOS in Trustzone at STM32L562ZET6Q.I want to use FreeRTOS in Non-Secure Zone.So, I enabled FreeRTOS in Middleware division.And, I want to change about Timebase Source in SYS_NS.But, all timers are disabled(in...
Kudos from
Kudos given to