STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1591 Views
  • 0 replies
  • 2 kudos

Ethernet-TCPip Nucleo F429ZIT6

Posted on April 06, 2017 at 13:14Hi,I use STM32CubeMX to generate the configuration of LWip on my card (nucleo F429ZIT6). Once my card program, I address a fixed IP address but I can't see my card on the local networks.The code generated is :int mai...

STM32-MAT Simulink problems

Posted on March 16, 2017 at 13:08I am trying to get the STM32-MAT package to work with Simulink to do some test on a stm32f4discovery board and I am running into multiple issues.1. A simple Simulink setup for a normal build:When building this simple...

0690X00000606a4QAA.png 0690X00000606aOQAQ.png 0690X00000606DdQAI.png 0690X00000606XzQAI.png

Touch Sensing with CubeMX and stm32l152-discovery

Posted on September 16, 2016 at 22:59I'm really struggling to get Touch Sensing working on the stm32L152 RCT6 discovery board. I'm trying to use it with CubeMX and understand that there is a particular procedure to use the Touch lib with CubeMX. Cou...

Cube MX Timer init Error on STM32F050R8

Posted on April 04, 2017 at 16:29Using the attached cube project TestSTM32F051R8_TimError.iocWhen I generate the source codes the CubeMx version  4.20.0 produces the following initialization code for the timers (I used only TIM1 and TIM3) but the er...

STM32F4 Memory Card Interface Issue

Posted on February 22, 2017 at 14:43Hello. I am trying to integrate SD Card (Transcend 4GB) with STM32F407 Disc board. I had followed all previous discussion & made corrections yet i am getting Error. I have attached my clock configuration, Pin diag...

Resolved! CubeMX creates broken SystemClock_Config()

Posted on November 04, 2016 at 13:42 In STM32Cube MX 4.17 I have set up an empty STM32L476 Nucleo project with and created code for the Low-Layer API. The parameters were: LL_PWR_REGU_VOLTAGE_SCALE2LL_RCC_MSIRANGE_8 The function System...

STM32CubeMX 4.19.0 Code generation issue

Posted on February 26, 2017 at 19:34Hi.I have noticed some problems when generating code using STM32CubeMX 4.19.0. I included the zipped project in the attachments. In the Src/main.c file it generates the declaration of the FSMC init functionstatic ...

petoknm by Associate II
  • 2532 Views
  • 4 replies
  • 0 kudos