Posted on February 26, 2017 at 19:34Hi.I have noticed some problems when generating code using STM32CubeMX 4.19.0. I included the zipped project in the attachments. In the Src/main.c file it generates the declaration of the FSMC init functionstatic ...
Posted on June 18, 2016 at 11:21HiI have previously worked with STM32CubeMX and I remember downloading it was easy. But now when I go to the website I go to the GET SOFTWARE section and there is no way of downloading it. I reinstalled my OS and I ne...
Posted on February 07, 2015 at 18:42
Hi
I want to receive data from ESP8266 module after restarting it. But after restart, it starts the communication at a higher baud rate and after it's done booting it uses 9600 baud. When I have the UART p...
Posted on August 23, 2014 at 09:52
Hi,
I am using a custom board withSTM32F401RB MCU and I want to run it at 84MHz from PLL<-HSE configuration. I have an 8MHz crystal on the board. But I don't know how to do it. I ran the STM32CubeMX (I don't...
Posted on February 27, 2017 at 21:39I should have specified that I encountered the issue on Linux. Now I tested it on Windows and it seems to work fine. Can you please test it on Linux?