STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1542 Views
  • 0 replies
  • 2 kudos

Resolved! SPI clock bypass option missing

In the SPI options for STM32H7S3, the "Prescaler (for Baud Rate)" drop-down box has various values from 2 to 256, but the option to bypass the prescaler is missing.To be clear, I'm referring to the BPASS bit in register SPI_CFG1:To get around this, I...

SteveMelnikoff_0-1752585327678.png

Resolved! OpenAMP issue on STM32H745

Software: CUBEIDE:1.18.0Firmware: STM32Cube_FW_H7_V1.12.1 Board: NUCLEO-H745ZI-Q The problem is as follows: when using this chip for dual core communication, reproducing according to the example given by ST, communication cannot be carried out no mat...

MECHO_0-1744812753218.png
MECHO by Associate III
  • 6239 Views
  • 18 replies
  • 1 kudos

ioc switching

hi I'm using nucleo-h755 144 pin board, i have configured for the project, now I'm changing the mcu from stm32h745BITx 208 pin package. is there any option in stm32cubeide to import the configuration from one mcu to another mcu in cube ide without or...

STM32U545 CubeMX TrustZone Starter Config

Hello,I have an existing project and I'm attempting to retrofit it with TrustZone, starting with a new IOC file that will be the basis of the project which I will then retrofit my code into. I'm starting with a clean slate ioc file for the STM32U545C...

JTR by Associate
  • 1089 Views
  • 0 replies
  • 0 kudos

Using DMA with UART Idle Timeout on STM32G4

Hi Team,I'm currently transitioning from using UART interrupt with timeout to DMA-based reception on an STM32G4 controller. I’d like to implement a similar behavior where I can detect the end of a UART message using idle line detection while receivin...

Failed in update the firmware package for STM32H5

I download the latest firmware package "stm32cubeh5-v1-5-0.zip" for STM32H5, from ST's website. I followed following instructions to install it via STM32CubeMX:Open STM32CubeMX.  Go to Help > Manage embedded software packages.  Choose the desired STM...

WenLiu_0-1752236346137.png
Wen-Liu by Associate
  • 1057 Views
  • 2 replies
  • 0 kudos