STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1570 Views
  • 0 replies
  • 2 kudos

CubeMX - User Code sections are deleted after regeneration

Hi,I am generating the basic initialization of my projects code with CubeMX. As far as I understood it, the user can insert "USER CODE" sections to prevent the automatic code generator from overwriting these code blocks.In my case, I want to prevent ...

JAlth by Associate
  • 710 Views
  • 0 replies
  • 0 kudos

Enable FreeRTOS Queue Sets in CubeMX

I am developing firmware for the STM32F413 that uses FreeRTOS, and I need to create a queue set. Thus far, I have been unable to find a way to enable queue sets in CubeMX. Obviously I can manually go into FreeRTOS.h and change the configuration const...

USB MSC and FatFS on the same mass storage device

Hi,for my current project, I like to use the FatFS library to read/write data to an SD card, connected to a STM32F429 through SDIO interface. This generally works and I can create/read/write files on the SD card.In addition, I like to use USB mass st...

JAlth by Associate
  • 1469 Views
  • 0 replies
  • 0 kudos

HAL_Delay issue

This has been posted in the "Community" space but actually belongs here. -- pahttps://community.st.com/s/feed/0D50X00009nLfs2SAC

Pavel A. by Super User
  • 705 Views
  • 0 replies
  • 0 kudos

STM32CubeMX code generation error

Posted on November 09, 2015 at 11:52When generating MX_Device.h with CubeMX for a STM32F407 device, the following pin names are illegal, because there is minus sign in the name:/* Pin PA13 */&sharpdefine MX_SYS_JTMS-SWDIO_Pin                   PA13/...

Why CubeMX generated code wipes out USER CODE areas ?

I use the latest STM32F4CubeMX and latest TrueStudio and updated firmware library. I have chosen in the Project Settings "code generator" option "Keep User Code when re-generating" but it does not. User code is strictly within the USER CODE labeled ...

eBirdman by Senior II
  • 867 Views
  • 2 replies
  • 0 kudos

Problem with VCP USB FS and CubeMX STM32H7eval

Hello, everybody.I'm trying to implement USB FS on STM32H734 eval board. I'm using CubeMX to generate code, the version is up to date and i'm using the latest firmware libraries (which is 1.3.0). I generated a standard project and configured a VCP on...

Simon1 by Associate
  • 1522 Views
  • 3 replies
  • 0 kudos