STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1570 Views
  • 0 replies
  • 2 kudos

Resolved! Bug in STM32H7 1.3.0 ADC multimode.DualModeData

I am using a STM32H7 ADC in multimode. When I generate the source code with STM32CUBEMX 4.26.1 and STM32CubeH7 Firmware Package V1.3.0 / 04-July-2018, i noticed that inside MX_ADC1_Init() in main.c, the following line of code is written:multimode.Dua...

MaxR by Associate II
  • 1787 Views
  • 2 replies
  • 1 kudos

STM32CubeMX 4.27.0 deletes empty folders

The latest version of the STM32CubeMX 4.27.0 deletes empty folders in my project structure during project generation.This is a nice feature if it deletes only previously generated folders that are not used any longer, but it also deletes folders that...

BUG: CubeMX 4.26.1 (Eclipse plugin): HSE_VALUE not set correctly

I have a project which is using an 11.0592MHz external TTL oscillator, PLL'd up to 66MHz HCLK.CPU is an STM32F303RET6 on a Nucleo-64 F303 board.IDE is Atollic TrueSTUDIO STM32 Edition.I found the System Tick timer was ticking at ~700us. After single ...

Phil1 by Associate II
  • 2133 Views
  • 3 replies
  • 2 kudos

I hope that the STM32CubeMX code generation tool can add user-defined keywords to ensure that the user's own added code STM32CubeMX is not deleted when the code is generated.

for example:​“/* USER CODE BEGIN Includes */   ..../* USER CODE END Includes */​/* USER CODE BEGIN 0 */.../* USER CODE END 0 */�?I found that these keywords only work for this definition in the generated code, but after I added them in the original l...

JLee.0 by Associate III
  • 2769 Views
  • 7 replies
  • 0 kudos

Regarding Issue in GPIO intruppt

I am Working on interrupt with gpio where Rising edge to be detected..i think i have Configured the Interrupt properly but it is not working ,,,I am Making pC13 as gpio because it is connected to a button,when i press the button interrupt should come...

NMuth by Associate II
  • 902 Views
  • 1 replies
  • 0 kudos

STM32F030K6T6 PA9

We are using ​STM32F030K6T6 PA9, PA10 for UART TX and RX. The BSP is generated using CubeMX, we can see the PA9 does not transmit, if we enable reversal in the BSP, then we can see that PA10 transmits but PA9 does not receive.​If we use PA2, PA10 for...

LSari by Associate
  • 797 Views
  • 1 replies
  • 0 kudos

Resolved! Analog reading 3 pins after each other

I have F303RE.The pin config are:The ADC config is:The Adc init code is generated as well the Analog Gpios. That is not a problem.I want to read one after each other. I added a function to select to config, but I dont know what SHould I pass the rank...

0690X000006C3hYQAS.png 0690X000006C3hdQAC.png
Marius CO by Associate III
  • 1329 Views
  • 3 replies
  • 0 kudos