No, it didn’t help, this was far to simple!I am looking for a safe way to detect if somebody is connected to the CDC interface, i.e., that a program on the PC has opened the VCOM UART connection. Pls. advice?
Thanks!But I newer succeeded in installing FUXv1.0.1 (-r32 0x20030030 1 -> 01000100 ), maybe the "stm32wb5x_FUS_fw.bin" in STM32Cube_FW_WB_V1.1.0 isn't this new one...
I see the same problem. Full log below... ------------------------------------------------------------------- STM32CubeProgrammer v2.1.0 -------------------------------------------------------------------USB speed : Full Speed (12MBit...