STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1578 Views
  • 0 replies
  • 2 kudos

Problem creating new TrueStudio project for STM32L053 (and I assume all STM32L0 parts) in STM32CubeMX v5.0.1

I updated CubeMX to 5.0.1 today, then created a new project for the Nucleo-64-STM32L053 board. I'm using Atolic TrueStudio for STM32 v9.2.0 as the IDE and toolchain.I set up the project for the board, selecting and configuring peripherals, along with...

STM32CubeMX error during project generation

Hello! I use CubeMX ver.5.1.0 and Linux Mint 19. When i push the button "Generate code" CubeMX creates source files and headers, but doesn't creates any project files or makefiles. Than it shows error message(screenshot in attachments). It shows this...

0690X0000089LYsQAM.png
RAkma by Associate II
  • 2227 Views
  • 4 replies
  • 0 kudos

FATFS Code Generation for STM32L (CubeMX)

I am using STM32L476VG and I want to write files to a SD card. In CubeMX I generate code for the FAT File System with the following settings:Moreover, I am using FreeRTOS with static memory allocation only:However, I have found two issues so far:Sinc...

0690X000006ByBOQA0.png 0690X000006ByBYQA0.png
OHaal by Associate II
  • 2473 Views
  • 4 replies
  • 0 kudos