STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1570 Views
  • 0 replies
  • 2 kudos

Resolved! CubeMX and LwIP : DHCP packet is sent, but something is wrong

Hello,I'm trying to get DHCP working as an initial step in using LwIP. Have generated project with CubeMX and now I'm catching the problem. Using Wireshark, I can see that DHCP Discover packet is sent, but no response is received. IT seems that somet...

bully by Senior
  • 1972 Views
  • 1 replies
  • 0 kudos

Resolved! Problem: If I set RTOS task priority to value higher than osPriorityNormal causes a Hard Fault when running on STM32F47xx. Has anyone else encountered this?

I'm running CubeMX 5.1 with FW_F4 V1.24.0 and Atollic TrueStudio 9.3.0. I have eleven RTOS tasks defined in CubeMX, but only one is actually invoked with its StartTask routine. As long as the priority on the task is osPriorityNormal(0) or lower, th...

cjwilde by Associate II
  • 2464 Views
  • 3 replies
  • 0 kudos

Does STM32F373 work in CAN Slave mode?

I am trying to implement CAN between two STM32F373, with one as master and another as slave. The problem I am facing is that it cannot be configured in slave mode. I am using Cube MX to create the initial configuration.When I configure in slave mode ...

0690X000006C42WQAS.jpg 0690X000006C42MQAS.jpg

STM32L4R5QII6P missing in STM32cubemx and not available to buy.

Hello,i want to design a board around STM32L4R5QII6P. It is not listed in STM32cubemx tool. Another issue is the lack of availability of this chip with any distributor. Similar controller without dedicated Vcore pins is available (part number STM32L4...

NAshr by Associate
  • 996 Views
  • 0 replies
  • 0 kudos

Resolved! TIM3 as Timebase Source on STM32F302RB

I recently switched an older project to CubeMX 5.1.0 and the F3 firmware package V1.10.0. We used freeRTOS and tim3 as the timebase source as tim1 and tim2 are already in use. The program does not pass the initial timebase configuration any more and ...

Blacbird by Associate II
  • 2259 Views
  • 4 replies
  • 0 kudos

Attempting to read/write to SD card via SDIO on STM32F

I'm trying to read and write to a microSD card using this reader from sparkfun https://www.sparkfun.com/products/12941 and a nucleo board with a STM32F429ZIT6U MCU via SDIO interface. I created the project through CubeMX V 4.21 (I used the most curre...

0690X000008AvtzQAC.png
RRayb by Associate II
  • 3778 Views
  • 5 replies
  • 0 kudos

Questions about 9-bit RS485 Multiprocessor Mode and HAL.

I am working on a project which is an upgrade of an existing project. The existing project was done with an Atmel processor, the current upgrade is based on an STM32F767. The project involves, among other things, multiple serial busses communicatin...

SBurc by Associate II
  • 3090 Views
  • 7 replies
  • 0 kudos