STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

UART Recive for unknown length

I am using STM32F103C8T6 MCU and STM32CubeMx.I currently reciving data from UART and printed on PC's serial but it will work only when data terminated by '\n' character.But what if the data from uart not terminated with '\n'??Can anybody help??Please...

JPanc.1 by Associate II
  • 997 Views
  • 4 replies
  • 0 kudos

FreeRTOS v10 - Malloc retruns 0.

Hello community,I'm working with a NUCLEO Board F767ZI and I use cubeMX to generate the project.My project is created with cubeMX 5.2.0 and I use FreeRTOS v10.0.1Now I have a problem with malloc function, inparticular, with this new FreeRTOS version ...

FedeRico1 by Associate II
  • 1164 Views
  • 1 replies
  • 0 kudos

The option 'generate code as pair of .c/.h files per peripherals and middleware' does not seem to work (at least for Keil MDK-ARM)

When selecting this option in the Project Manager section of CubeMX, the build process in Keil generates a linker error:.\Objects\Aeolics.axf: Error: L6218E: Undefined symbol MX_GPIO_Init (referred from main.o)..\Objects\Aeolics.axf: Error: L6218E: U...

Resolved! STM32L431KBU6 - can't get past clock initialization

Hi!I'm just starting learning STM32, I got a st-link cutoff from a nucleo-board. I find programming ready boards a bit boring, so I went straight to naked MCU on breakout boards.So I got this STM32L431KBU6 chip on breakout and I can't get it to star...

0690X000008BEo0QAG.png 0690X000008BEpDQAW.png 0690X000008BEojQAG.png

STM32CubeMX / STM32CubeIDE100 - Recommendations

In the build-in CubeMX, there are some improvements possible:Unable to alter some pull-down boxes in the Clock Configuration, they disappear when trying to move the mouse to the desired selection (must use cursor and enter keys instead)When selection...

Jack3 by Senior III
  • 591 Views
  • 0 replies
  • 0 kudos

UART DMA Transmit and receive not working

I'm using Atollic True Studio V 9.0 , CubeMx v5.1.0, STM32F407VG-DISC1 board and enabled DMA for UART2. My code:int main(void) { int i = 0; HAL_Init(); for(i = 0; i<10; i++) rx_arr[i] = 0; for(i = 0; i<10; i++) tx_arr[i] = i*2;   SystemCl...