User Activity

I am evaluating MEMS sensors using the SensorTile hardware and accompanying software (STSW-STLKT01). The toolkit has thus far been very nice. In order to move the project further I now want to port the AudioLoop example project to another MCU on a Nu...
I am exploring the SensorTile (STEVAL-STLKT01V1) and would like to capture Audio recordings on a Unix OS (namely Raspbian). I have looked through the documentation here and the option to save audio to SD card is not ideal for my application, neither...
Hi,I am trying to record audio on a STM32F412 with an MP23DT05-A (digital MEMS microphone made by ST) using DSFDM.After basic configuration in CubeMX the project does not compile. The error is a missing function: undefined reference to `__HAL_RCC_D...
Dear ST community,We are running a CAN network with a lot of nodes (>200) using the STM32F107VCTx chip (and MCP2551 transciever) all receiving instructions from a central linux embedded computer with a MCP2515 CAN Controller.Sometimes the nodes stop ...
I have FreeRTOS set up on an STM32F107 performing several tasks of different priority in "parallell". There is one task of IDLE priority that blinks an LED and one task of Normal priority that receives communication over CAN (triggered by external i...
Kudos from