CubeMX 4.26.1 Makefile project generation bug?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-09-10 8:46 PM
When a TSC is selected, CubeMX populates two lines of the same source file in the Makefile. In other words, there are two lines of:
Drivers/STM32L0xx_HAL_Driver/Src/stm32l0xx_hal_tsc.c
in the Makefile created by CubeMX. To reproduce, create a new project with a L0 device, select TSC with some channel settings, and generate a Makefile project.
Another bug is that CubeMX failed to update existing Makefile. To reproduce this bug, simply open up existing Makefile project file (*.ioc) and try to regenerate it.
Labels:
- Labels:
-
STM32CubeMX
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0