STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1575 Views
  • 0 replies
  • 2 kudos

Does not add arm_math.h in new version

Hello. Speaking of more stuff broken with the new update.I tried to update a project for an assignment, just wanted to change some peripheral settings and here comes the warning about downloading new version. Okay then.But now the generator does not ...

LAfon by Associate III
  • 1987 Views
  • 3 replies
  • 0 kudos

__weak functions in stm32XXxx_it.c

Is it possible to fix the CubeMX so that when it generates the code for STM32 chips it will add __weak declration to the following functions:SysTick_HandlerPendSV_Handlerinside stm32XXxx_it.cWhile intergrating to embOS, the OS api overrides these fun...

ONaor by Associate
  • 912 Views
  • 0 replies
  • 0 kudos

How to select STM32H7 CubeMX LL drivers

Hi,STM32CubeMX H7 firmware version 1.4 includes LL drives, but how do you select them in CubeMX? Specifically for the LPUART.Only the HAL selection shows up for an existing and newly created project. See screen shots.Thanks.

0690X000008BXyjQAG.png 0690X000008BXyeQAG.png

DMA CubeMX enabling for HAL_SPI_TransmitReceive_DMA()?

Hi there,I am currently using the HAL_SPI_TransmitReceive() function for back-to-back read/write with a GPS modem as the slave. If i want to now implement the SPI coms with DMA, what is the correct DMA channel config in CubeMX?Only one DMA channel is...

NA1 by Associate II
  • 1417 Views
  • 3 replies
  • 0 kudos