cancel
Showing results for 
Search instead for 
Did you mean: 

bugfix: STM32cubeMX uses uninitialized memory for LL_USART_Init

ingo donasch
Associate
Posted on July 10, 2018 at 09:49

When generating MX_USART1_UART_Init for a usart in HalfDuplex mode, the USART_InitStruct.HardwareFlowControl field remain uninitialized  which leads to unpredictable behavior of the system. in my case the I2C DMA was triggered by  USART DMA requests....

fix: adding the missing initialization fields in mcu/config/llConfig/USART-STM32F0xx_LLConfigs.xml fixes the issue.

I only fixed this for my F030F4 project, the same issue might also be present for other configurations/mcu's

regards

ingo

#stm32cubemx-bug-ll_usart_init #stm32cubemx-bug
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Imen.D
ST Employee
Posted on July 11, 2018 at 15:42

Hello

idonasch

Can you please precise which CubeMX version are you using?

Please share your ioc file to check this issue.

With Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on July 11, 2018 at 19:49

Sorry for not providing this information in the first place:

STM32CubeF0 Firmware Package V1.9.0 / 25-August-2017

STMcubeMX V1.0 Version 1.0

adding the missing HardwareFlowControl entries to

'mcu/config/llConfig/USART-STM32F0xx_LLConfigs.xml'

fixed the problem (see attachment patch.txt). But this is not a complete fix! I only patched a few obviously missing entries in the supplied version and only for this mcu.

issue was in Src/usart.c:

...

<quote>

void MX_USART1_UART_Init(void)

{

// <<<<<<<<<<< The following struct is left uninitalized >>>>>>>>>>>>>>>

LL_USART_InitTypeDef USART_InitStruct;

LL_GPIO_InitTypeDef GPIO_InitStruct;

/* Peripheral clock enable */

LL_APB1_GRP2_EnableClock(LL_APB1_GRP2_PERIPH_USART1);

/**USART1 GPIO Configuration

PA2 ------> USART1_TX

*/

GPIO_InitStruct.Pin = LL_GPIO_PIN_2;

GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;

GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH;

GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_OPENDRAIN;

GPIO_InitStruct.Pull = LL_GPIO_PULL_UP;

GPIO_InitStruct.Alternate = LL_GPIO_AF_1;

LL_GPIO_Init(GPIOA, &GPIO_InitStruct);

/* USART1 interrupt Init */

NVIC_SetPriority(USART1_IRQn, 1);

NVIC_EnableIRQ(USART1_IRQn);

USART_InitStruct.BaudRate = 38400;

USART_InitStruct.DataWidth = LL_USART_DATAWIDTH_8B;

USART_InitStruct.StopBits = LL_USART_STOPBITS_1;

USART_InitStruct.Parity = LL_USART_PARITY_NONE;

USART_InitStruct.TransferDirection = LL_USART_DIRECTION_TX_RX;

>>>>>> USART_InitStruct.HardwareFlowControl = LL_USART_HWCONTROL_NONE; <<<<<< // THIS LINE WAS MISSING

USART_InitStruct.OverSampling = LL_USART_OVERSAMPLING_16;

LL_USART_Init(USART1, &USART_InitStruct);

LL_USART_ConfigHalfDuplexMode(USART1);

LL_USART_Enable(USART1);

}

</quote>

originally the marked line was missing leaving the 'USART_InitStruct.HardwareFlowControl'

entry uninitialized. this eventually led 'USARTx->CR3' to be modified through a

WRITE_REG((REG), (((READ_REG(REG)) & (~(CLEARMASK))) | (SETMASK)))

where CLEARMASK was (USART_CR3_RTSE | USART_CR3_CTSE)

but SETMASK contained random stack-values and in my case the DMA bits had been asserted, swamping my I2C tx register because USART1 & I2C1 share the same DMA channel....

bugs of this kind are very hard to debug, so please evaluate all other XYZ_InitStruct for complete initialization for all combinations of MCU's.

thanks for taking care of this issue

regard

ingo

ps. an email reply bounced....

________________

Attachments :

MSB2optima.ioc.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HxQh&d=%2Fa%2F0X0000000axv%2FsokmivXZN4SePbpml4KfMpMbfXoJqwwjOuv2lXJhuEg&asPdf=false

patch.txt.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HxQc&d=%2Fa%2F0X0000000axu%2F4x16dl2nA.ZhmAqHynuxQFuwMYI3.CcqPDZUBQry7_c&asPdf=false
Nawres GHARBI
ST Employee

Hi could you please attach the ioc and tell me which version of STMCubeMX are you using please?

Tested with the 4.26.1 and all is working good