STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1584 Views
  • 0 replies
  • 2 kudos

Generate adjustable single short pulse (using timer ?)

Hello,I want to generate a single short pulse (adjustable between 100 ns to 1ms). What is the best way ?I think we should use timers, but which mode ? (which CubeMX configuration ?)Moreover I tried to configure one-pulse mode but I can't find documen...

SDMMC1 on stm32H743ZI _ fails!

Hi, i need help in my project. I have a problem with SDMMC1 and fatfs. My goal is to be able to write a txt file on the sd cardDoes someone have an example that works correctly?im using stm32cubemx 5.2.1 and atollic ide.thanks

dresc by Associate II
  • 863 Views
  • 2 replies
  • 0 kudos

Problem with STM32F4 External Interrupt executes repeatedly

Dear All,i encountered a problem with STM32F407ZGT6 in working with external interrupt.i do this by STM32CubeMX and MDK ARM V5.i configure a pin ( PF1 ) as external interrupt mode with rising/falling edge trigger detection. i set it internally pull d...

RShar.17 by Associate II
  • 3369 Views
  • 4 replies
  • 0 kudos

CubeMX USART DE config incorrect - STM32F091

Using RS485 driver enable, specifically on USART 7 and 8, the CubeMX generated code needs to add in MspInit:GPIO_InitStruct.Alternate = GPIO_AF1_USART7;GPIO_InitStruct.Alternate = GPIO_AF2_USART8;respectively.

IHave by Associate
  • 646 Views
  • 0 replies
  • 0 kudos