STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

Bug Sys Debug disable on MX_Cube_5.4

Hello, After update the CubeMX from 5.3 to 5.4, and I change the IOC and generate a new code, a error appear and debug is disconnected. Before the update:After the update:I doesnt change nothing in the code, just change a GPIO_Input to Output.I insta...

0690X00000ArnWqQAJ.jpg 0690X00000ArnX0QAJ.jpg
joaoleao by Associate II
  • 610 Views
  • 0 replies
  • 0 kudos

Where to report bugs in the STM32CubeMX?

It seems the clock configuration is not generated correctly by the Cube.Used STM32CubeMX Version 5.2.1 for STM32G070RBT deviceThe root cause seems to be the RCC_CCIPR_TIM1SEL is not defined.As a consequence the RCC_PERIPHCLK_TIM1 is not available and...

Andi by Associate III
  • 1625 Views
  • 3 replies
  • 0 kudos

Code Generation Bug in STM32CubeMX ? Unable to generate UART (one wire half-duplex mode) pin configuration, resulting in the inability to use UART.

MUC: STM32G031G8UxSTM32CubeMX version: 5.4.0Package version: STM32Cube FW_G0 V1.3.0Keil version: v5.28--------------------------------------------------------------------void MX_USART1_UART_Init(void){ huart1.Instance = USART1; huart1.Init.BaudRate =...

0690X00000Arfm7QAB.png 0690X00000ArfmWQAR.png

STM32F070RB USB MSC on internal Flash can not format

Hello,everybody Nice to meet you,My trouble is "STM32F070RB USB MSC on internal Flash can not format " ..I have try some idea in community but did not help,so I decided to ask for help,Here are my code on usbd_storage_if.c.Thank you so much !#define ...

0690X00000888T9QAI.png