STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1628 Views
  • 0 replies
  • 2 kudos

Resolved! UARTs GPIO speed can be low?

Noticed that new Cube versions and CubeIDE, generate initialization code for UARTs TX and RX pins with GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOWPrevious Cube versions (at least 4.x) generate instead GPIO_SPEED_FREQ_VERY_HIGH.Was this change intenti...

Pavel A. by Super User
  • 2052 Views
  • 2 replies
  • 0 kudos

lwip update to current version

Hi,regarding the lwip stack in cube-mx (currently 5.4) the version is fixed at 2.0.3 .Is there a plan to move on to the current version 2.1.2 of the stack?If not, are there any known pitfalls, when manually migrating the underlying stack to another v...

JRS by Associate III
  • 2929 Views
  • 5 replies
  • 0 kudos

When I use CubeMX to generate a middleware USB HID device I can enumerate successfully with a Nucleo-144 board. However, when I try the exact same setup except use the custom HID option the device manager reports Error 10

Error10 = "Extra end collection found or end collection not found". CubeMX version 5.4.0 Compiling under IAR version 8.40. NUcleo-H743Z. Heap is set to 0x1000 per forum post.

FScha by Associate
  • 787 Views
  • 0 replies
  • 0 kudos

STM32CubeMX v5.4.0 unable to generate Keil5 code

helloYesterday I was update my cubeMX to v5.4.0 and I trying generate any code and that was showing popup error : "The Code is succesfully generated under: <project localization> but MDK-ARM V5 project generation have a problem."The strange think is ...

mystmyst by Associate
  • 1039 Views
  • 0 replies
  • 1 kudos

About stm32f429 with 1bit SDIO with FATFS working perfectly but 4 bit SDIO with FATFS is not working generate error FR_DISK_ERR also generate FR_NO_FILESYSTEM

i am use NUCLEO -F429ZI Bord stm32cubemx 5.4.0 with atollic truestudio 9.3.0 and also stm32cubeide 1.1.0 i will use our customized SD CARD SDIO BORD i will make code for SDIO1 bit SDIO with FATFS will work perfectly at system freq180mhz and SDIO freq...

pragnesh by Associate III
  • 1289 Views
  • 2 replies
  • 1 kudos

Resolved! UART2 on Virtual COM works but UART1 does not

Hi everyone,Figured I banged my head against a wall long enough, so might as well ask even if it is a really simple fix.So far I have only used USART2 to write data to the Virtual COM port from my nucleo board, now I have need to write other data out...

L4CAJS by Associate II
  • 6535 Views
  • 9 replies
  • 0 kudos

I'm running the Ac6/Eclipse environment on a Mac with the STM32CubeMX plugin installed. I recently updated the MX to the latest and it installed 5.1.0. Is 5.4.0 not available as the plugin? In the release notes, it says the latest compatible Cube FW is

In the release notes, it says the latest compatible Cube FW is 1.24.0. But Cube FW 1.24.1 is listed at a patch. So which should I install with STM32CubeMX 5.1.0?When I start STM32CubeMX in its perspective I get a popup with the message "This release ...

Ron Koch by Associate II
  • 897 Views
  • 0 replies
  • 0 kudos