STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1584 Views
  • 0 replies
  • 2 kudos

STM32L552E-EV and STM32Cube_FW_L5_V1.1.0

Hello,I have a STM32L552E Evaluation Board, and I see that the Examples and Applications folders have projects for IAR, KEIL and CubeIDE. Previusly I used System Workbench for STM32, so I installed CubeIDE and I tried to run and debug some code in th...

Why Nucleo L053R8 crashes after 7~11 minutes of execution?

I'm using STM32CubeMX 5.2.0MCU: STM32L053R8TxFirmware: STM32Cube FW_L0 V1.11.2Toolchain/IDE: MDK-ARM V5Tested with 3 different boards, even with a default code (as generated by CubeMX) in debug mode, and also with a simple UART transmitter program (t...

elyes by Associate
  • 2179 Views
  • 4 replies
  • 0 kudos

Hardware Reset Affecting Input Capture Direct?

Hi,I have come across an unusal problem and I can't seem to figure out.I am using an RC transmitter to send signals to a receiver that is hooked up to an STM32F411VE board. I am reading the receiver signal using input capture direct mode (timer 2, ch...

0690X00000BwM9yQAF.png
GEvan.1 by Associate
  • 1297 Views
  • 1 replies
  • 0 kudos

I am trying to build up a QSPI connection with the STM32H7 Nucleo Board (H743zi2). I generated the keil project(setup with CubeMX). Am measuring the CS and CLK with my oscilliscope & I cant see anything for QSPI clk more than 30MHz.

I have attached the main file.I am using nucleo 144 board and have setup the stm32 core for 480MHz(max), so max QSPI clock allowed is 240M/2=120MHz. But am not able to generate clock pulses if I set QSPI clock prescalar less than 8 (30MHz). I have tr...

Sk.2 by Associate II
  • 7722 Views
  • 9 replies
  • 0 kudos

How to connect 8 mems microphones to DFSM using 4 filters?

Hello! I am using a stm32f765 chip. I need to connect 8 microphones to the DFSDM, but there are only 4 filters in the chip and I cannot use the regular read mode from all 8 channels of the DFSDM. I found information that the dfsdm filter allows to re...

RTolm.1 by Associate
  • 1099 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeMX V4.24.0 code generation failure (bug report)

Posted on February 13, 2018 at 18:23ST: Bug report:I've just upgraded from CubeMX V4.23.0 to V4.24.0.Using this re a Nucleo 144 'F767 board, I'm finding that 'Menu => Project => Generate Code' works once, then fails thereafter in one of two ways:If '...

JB2500 by Associate III
  • 7220 Views
  • 9 replies
  • 0 kudos