cancel
Showing results for 
Search instead for 
Did you mean: 

Why can't I enable all 4 SAI ports on STM32H750/STM32H743?

caleb
Associate III

Hello,

I am attempting to use all 4 sai ports as one large synchronous audio device.

The I want SAI1A to be the master, and SAI1B, SAI2A, SAI2B, SAI3A, SAI3B, SAI4A, SAI4B to all be synchronous slaves to the SAI1A.

I am able to configure them all, except for SAI4B, which says it's in conflict with SAI1B synchronous slave. I'm using the internal synchronous signals, all synchronous slaves are marked as, "Synchronous with other SAI, SAI1". But just 4B says it's in conflict.

I assume if I configure it manually, it'll probably work fine...

Thanks

-Caleb

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Amel NASRI
ST Employee

Hi @caleb​ ,

This issue seems to be similar to the one reported in this question.

I add @Khouloud ZEMMELI​  to let us know if there is any update on this regard.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

​Hello , For : this question : According to our development team, the product supports only 6 microphones.

Request invalid.

Regards,

Khouloud.

Khouloud ZEMMELI
ST Employee

​@caleb​  , could you please share more info about your request? which version of CubeMX?

Regards,

Khouloud.

Khouloud ZEMMELI
ST Employee

hi ​@caleb​ , Tested with H743IIKx and it works fine , for H750 it will be fixed .

Best Regards,

Khouloud.