STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

FSMC PSRAM setup time

Hello, I am trying to test PSRAM memory on STM32L4R9-Discovery board (STM32L4R9AI), I still don't understand how to calculate the PSRAM setup time (address setup time), (data setup time), (data hold time) and (bus turn around time) could someone expl...

RS485 Pin Configuration Conflict

Trying to understand this warning when configuring pins for a stm32g071RB in CubeIDE. Enabling the RS485 Hardware Flow Control even with no other peripherals enabled causes the warning to flag to display. The explanation message does not explain much...

AChen.1 by Associate
  • 960 Views
  • 0 replies
  • 0 kudos

Problem generating SW4STM32 Project on Windows 10

Hi,I use CubeMX to configure STM32 controllers (mostly STM32F746ZG for testing on a Nucleo-144 board, but also tried with other boards and single MCUs).Since I moved to Windows 10 64Bit, the generation of SW4STM32 projects does not work properly anym...

0690X00000Bw0n3QAB.jpg
SJaco.1 by Associate
  • 1373 Views
  • 1 replies
  • 1 kudos

Resolved! How install NFC5 package? not able to install

Hi, I am running STM32CubeMX 5.5.0 (newest)And downloaded the NFC5 2.0 expansion package from ST website, but when I try to install it in Cube it give me this error:How do I do to install it?I just got one NFC05A1 board to evaluate but got stuck in t...

0690X00000Bvy2eQAB.png

Errors when including "arm_math.h"

Micro-controller: STM32F407VGTCompiler: Keil V 5.28.0CMSIS Core Library: V 5.2.0DSP Library: V 1.6.0I need some help including the CMSIS DSP library in my project. I have included the CMSIS DSP library via Manage Run Time Environment, this links the ...

m_n by Associate
  • 4704 Views
  • 1 replies
  • 0 kudos

STM32CubeMX 5.5.0 released

What you have to know before migratinghttps://community.st.com/s/question/0D50X0000BztfjUSQQ/migration-issue-from-540-to-550What is new in STM32CubeMX V5.5.0?• Removed TouchGFX, STemWin, Graphics Selector and Simulator supports.The new solution based...

Resolved! Can Example Problem with CubeMX

Posted on June 04, 2018 at 08:04Hello,       I am trying to implement a canbus example. I was used can example with no problem in the CubeMX Version 4.24. Now, I have updated the CubeMX to version 4.25.1. Can exampel is not working now. There are so...

Resolved! NUCLEO-L476RG GPIO port D ?

When I generate code with CubeMX the MX_GPIO_Init code contains: /*Configure GPIO pin : PD2 */ GPIO_InitStruct.Pin = GPIO_PIN_2; GPIO_InitStruct.Mode = GPIO_MODE_ANALOG; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);There...

Lama by Associate III
  • 2589 Views
  • 4 replies
  • 0 kudos