STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1624 Views
  • 0 replies
  • 2 kudos

stm32h753 rtc resets after power down (vbat is connected)

Hello, I am using a stm32h753 and stm32cubemx, and trying to run the RTC module on VBAT. To do this I have connected a battery to the MCU. RTC is connected to LSE. Next, I set the RTC in my code and then I disconnect the MCU from power source, and th...

VYoun by Associate III
  • 1327 Views
  • 1 replies
  • 0 kudos

Lock-in detection on stm32f373cct6

I want to implement a lock-in detection on stm32f373cct6 that means that I need to trig the DMA of the DAC and the DMA of the SDADC with the same timer.I am using CubeMx to confugure the stm32f373cct6.I want to trig the DMA of the injected SDADC1 wit...

Resolved! SDRAM 32bit bus can't be selected for STM32H7

Hello,I'm trying to connect SDRAM to STM32 for the first time and I'm having trouble understanding the specs.In the datasheet, it seems the FMC peripheral can support 32bit memory.But when I use the Cube MX setting, I'm only able to select 16 bits fo...

0693W000000TquTQAS.png 0693W000000TqnXQAS.png
BHan.1 by Associate II
  • 2930 Views
  • 4 replies
  • 0 kudos

STM32L4 + SD + STM32CubeMX v5.0.0: SD clock speed during call to SDMMC_CmdSendSCR (as part of switch to 4-bit bus) is too fast for many SD cards

The function BSP_SD_Init() is called once the basic SD card initialisation is complete, and after the SD clock speed has switched from 400 kHz(*) to full speed.If the bus has been configured in Cube to use 4-bit mode, the following call chain occurs,...

What is the Problem with my Program? (Using Mat-Target)

@The things i use:Hardware: Stm32F446RESoftware: CubeMX V.5.4 ; Matlab R2019b ; CubeIDE V.1.1 ; Mat-TargetMy Question is: Where is the Mistake in my Programm. I defined the PA5 as a Gpio output because that´s the Output for the LD2 LED on my board wh...

Driko by Associate II
  • 5035 Views
  • 2 replies
  • 1 kudos

STM32CubeMX H7x5/H7x7 USB CDC bug

Hi there,I'm using the H7 dual core MCU's and using the M4 core for USB CDC.There is an issue with using the M4 core with USB CDC.The reference manual states at page 137 that address 0x1FF00000 - 0x1FF1FFFF is available to the M7 core as "System Memo...

Mvan .31 by Associate II
  • 2048 Views
  • 1 replies
  • 2 kudos