cancel
Showing results for 
Search instead for 
Did you mean: 

is it possible to configure three ADCs of the STM32F4, ADC1 and ADC2 in dual interleaved and ADC3 independent?

rsharifi9
Associate III

Dear All,

Please consider STM32F407. I tried to configured its three ADCs: ADC1 and ADC2 in dual intereleved and ADC3 in independent mode using CubeMX. BUT it is impossibe the job using that. Is it possible to moddify the CubeMX's generated code to work correctly? How can I do the project?

Regards, Rasool

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

I suspect it is possible, perhaps look at the HAL examples and adapt. Start with a Dual example, then fire up ADC3

For F4 I would have used the SPL

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
RShar.17
Associate II

I initilize the ADC in dual mode and independent mode separately but i don't have success in my application.

I think, there is no basically difference between my code and the one generated with CubeMX though both of them are based on HAL library.

What is the true initialization for these ADCs?

rsharifi9
Associate III

To be blunt, Cube often fails miserably for non-standard use cases. Don't put your trust in such auto-generated code.

You can either check check the Cube output and look for errors, or use your own code based on the reference manuals.

I don't know any reason why your setup should not work.

I always used the ADC independantly, though.