STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 2 kudos

Resolved! EXTI Triggering itself

Hi,I am working on a custom board using the STM32F479NI.I have been able to use EXTI on the PC7 without problems.Now I need to implement it on PE2.But this time, the EXTI2_IRQHandler is being called over and over without any electrical changes on tha...

0693W000000W74EQAS.png 0693W000000W7ChQAK.png 0693W000000W74tQAC.png 0693W000000W74sQAC.png
AMass.1 by Associate II
  • 4925 Views
  • 9 replies
  • 0 kudos

[BUG] SD Driver 4Bit Mode no DMA use

Hello,i switch from 1bit mode to 4bit mode in cubeMX (latest version on linux) an the reading only works in debug mode, when i connect my board to only power it doesn't work anymore.In CubeMX under SDIO the DMA2_RX and DMA2_TX is set to stream3 and s...

GIkar by Associate III
  • 4044 Views
  • 8 replies
  • 0 kudos

CubeMX: 0-Pointer access in generated MX_ETH_Init code

Hi!I've opened an issue on Github for the STM32H7 Cube HAL:https://github.com/STMicroelectronics/STM32CubeH7/issues/33Because the bug is in the CubeMX generated code, I hope this is the right Forum to report the bug.Best regards,Thomas

mail_st by Associate II
  • 1641 Views
  • 2 replies
  • 1 kudos

Failed to use STM32CubeMX+H743+SDMMC+DMA+FATFS

Hello. I am using CubeMX to generate project and code. Without using DMA I can write SD card successfully, while I enable DMA f_open will wait for 30 seconds ( timeout) and fail with an Error 1 output.The CubeMX project is in the attachment.I need yo...

wjiac.1 by Associate II
  • 1766 Views
  • 3 replies
  • 0 kudos

USB_OTG_HS Mass storage using internal DMA does not work

Hi all,I am implementing Mass Storage class device with USB_OTG_HS. The implementation is configured from CubeMX and works perfectly until I enable USB_OTG_HS internal DMA. As soon I do this everythig stops, and no functions from usbd_storage_if.c ar...

DmRozhd by Associate III
  • 1364 Views
  • 2 replies
  • 0 kudos

I am new of the bluetooth argument. My application is based on STM32F411. I need to communicate with an external HCI bluetooth board via UART, but I do not find the correct stack for doing that.

I try to configure my project by Cube MX enabling additional software X-CUBE-BLE2 as start point. When I try to compile I get the error "hci.h not found". I think something is missing, but all the code is Cube generated,Is there a ready to use HCI st...

GGuer.1 by Associate II
  • 2218 Views
  • 5 replies
  • 0 kudos

Bug in stm32l4xx_hal_conf.h template file

Hi, I just noticed that if Enable Full Assert option is enabled in the Project Manager, the generated stm32l4xx_hal_conf.h file has the following definition for assert failed:void assert_failed(char *file, uint32_t line);Which conflicts with the othe...

MVigni by Associate II
  • 3342 Views
  • 7 replies
  • 0 kudos