STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1570 Views
  • 0 replies
  • 2 kudos

Accidentally deleted program, can't restore it - very urgent

I created a CubeMX project in an important folder. I found out, that all the project files were not put inside an own folder and were all over the place. So I wanted to delete the Project to make a new one. When deleting i clicked on "delete project ...

LMess.1 by Associate
  • 2734 Views
  • 3 replies
  • 0 kudos

MBEDTLS / STM32CubeMX Broken?

I am trying to implement an MBEDTLS client based on an ST example. The MBEDTLS code fails when it tries to allocate memory using calloc. Apparently, users have been experiencing this for over a year.https://community.st.com/s/question/0D50X0000ArVXN...

CubeMX IDE v1.3.1, MacOS 10.14.6, Build fails with "/bin/sh: arm-none-eabi-objcopy.exe: command not found" - the ".exe" is incorrect.

The makefile is not correct with: arm-none-eabi-objcopy.exe -O ihex "IOproc.elf" "IOproc.hex", but the IDE is trying to run arm-none-eabi-objcopy.exe. I just reinstalled the IDE using the Mac installer - no change. How can I get the IDE to generate a...

TTeag.1 by Associate
  • 2141 Views
  • 3 replies
  • 0 kudos

Resolved! STM32Cube NUCLEO-F413ZH UART missing

Hello,I am trying to create a project with STM32Cube 5.1.0 for NUCLEO-F413ZH. I see only USART 1, 2, 3 and 6 available, none of the UARTs 4, 5, 7, 8, 9 and 10. These UARTs are available if I open a project for STM32F413ZHT, the device used in NUCLEO-...

AGoro.1 by Associate
  • 1367 Views
  • 2 replies
  • 0 kudos

Resolved! GPIO High-Speed Option - Not Available on PC13-15

Hi All,I am trying to set a few GPIO speed to High Speed but I was struct when PC13-15 are only able to set to Low Speed. May I know is this the STM32CubeMx bugs?Or it is the STM32F446RE limitation? Please help.Many Thanks

0693W000001rMFDQA2.png

STM32H7 CAN FD bit timing when configured as classic can

Hello, I need to configure the CAN FD in STM32H7 as classic can. However, I can not understand the bit timing explained in the reference manual. Can someone please help me to figure out the bit timing for a clock frequency of 42Mhz? Your help is much...

VYoun by Associate III
  • 3050 Views
  • 3 replies
  • 0 kudos

Resolved! CubeMX talks about Github, a link?

On the stasrt-op screen of Cube the is a picture/text about Github.I can't find any link to ST CubeMx on Github. I find a lot of links about Cube but they I dont think they what CubeMX talks about.

LMI2 by Lead
  • 2422 Views
  • 5 replies
  • 0 kudos