STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1572 Views
  • 0 replies
  • 2 kudos

Resolved! PWM output generation from NUCLEO-F031K6 (MCU: STM32F031K6) is not working. Code is generated from STM32CubeMx.

I'm using NUCLEO-F031K6 (MCU: STM32F031K6) for PWM output generation (100Hz clock). Project is generated from STM32CubeMx v5.6.1. PA11 (TIM1_CH4) is used for PWM output. No clock pulses are seen. APB1 timer clock is 8MHz. ----------------------------...

S.Kamath by Associate III
  • 878 Views
  • 1 replies
  • 0 kudos

ARM CMSIS 5.7.0

I've been trying to download the CMSIS 5.7 update for almost a month now.But when I try to download and install the library every day, I get errors in the file in the attached screenshot.Every day I hope that you have noticed the problem or that some...

RMent.1 by Associate
  • 1917 Views
  • 4 replies
  • 0 kudos

trying to operate an external interrupt on stm32f031k6

Im trying to operate an external interrupt on my STM32F031K6, using STM32cube IDE. Ive been following a tutorial here https://simonmartin.ch/resources/stm32/dl/STM32%20Tutorial%2007%20-%20GPIO%20Interrupts%20(EXTI)%20using%20HAL%20(and%20FreeRTOS).pd...

deep_rune by Associate III
  • 1286 Views
  • 1 replies
  • 0 kudos

Change peripheral ( USART ) config ( CubeMX )

Hi, by following some video i am able to create a GUI ( ST32F469I-DISCO ) and get a complete CubeIDE project... I create the GUI by selecting the right application template for the TouchGFX project ( device ). Then i can generate the code. After th...

LFili.1 by Associate II
  • 3245 Views
  • 4 replies
  • 0 kudos

Resolved! How to setup SMPS Supply source in STM32CubeMX?

Hi,I want to configure my STM32H7 MCU to use SMPS configuration.I try to select RCC -> Supply Source -> PWR_DIRECT_SMPS_SUPPLY, but then get build error Src/main.c:136:26: error: 'PWR_DIRECT_SMPS_SUPPLY' undeclared (first use in this function)This is...

Tuoman by Senior II
  • 9196 Views
  • 1 replies
  • 1 kudos