STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1647 Views
  • 0 replies
  • 2 kudos

The time-out time of flash operation is fixed 50000ms

I use STM32CubeMx to generate a project, in this project the FLASH_TIMEOUT_VALUE value is 50000ms by default.I want to know why STM32CubeMx set 50000ms as its value? It was used in this function:HAL_StatusTypeDef FLASH_WaitForLastOperation(uint32_t ...

Agao.1 by Associate II
  • 2051 Views
  • 3 replies
  • 0 kudos

Resolved! I want to use timer interrupt for some operations in my application.But i am unable to set the exact parameters for timer..I am using two timers...TIM7 for 1ms & TIM 14 for 20 ms...what should be the setting for prescaler & period?

Please find the details below:Part - STM32F072VBstm32cube mx for code generationtimer clock - 24MHzstatic void MX_TIM7_Init(void){ /* USER CODE BEGIN TIM7_Init 0 */ /* USER CODE END TIM7_Init 0 */ TIM_MasterConfigTypeDef sMasterConfig = {0}; /* USER ...

Bs.1 by Associate II
  • 2118 Views
  • 3 replies
  • 0 kudos

Resolved! RTOS. osMailQId bug.

I got an interesting bug when working with the queue (STM32CubeMX 5.6.1 + lib 1.25 in STM32F407VGT6):typedef struct{ uint8_t* data; uint16_t len;} message_t;uint8_t str[] = "hello\n"; for(;;) { message_t* message; if ((message = osMailAlloc(ComOutput...

0693W000003OqkkQAC.jpg
NorfLoud by Associate III
  • 1435 Views
  • 1 replies
  • 0 kudos

CubeMX seems to generate wrong code for RTC_OUT2

Target is the Nucleo G474RE board and I've tried both the CubeIDE (1.3.1) embedded CubeMX and the standalone CubeMX (5.6.0) in both cases if you enable the Calibration option and set it to "Calibration 1Hz routed to OUT2" then the signal comes out of...

Adding Additional Software Pack ARM.CMSIS 5.6.0 onSTM32H743, running on Nucleo H743ZI2, I get 'Incomplete Inclusion' error on all source files - Middleware folder.

Every time, I regenerate the code after including the above ARM file, I get an error on all source files that states 'incomplete inclusion' - enable CMSIS DSP. I have been getting around this by adding the appropriate ARM DSP libraries manually. ...

MLane.3 by Associate II
  • 3093 Views
  • 5 replies
  • 0 kudos

STM32CubeMX 6.0.0 released

What is new in STM32CubeMX V6.0.0?  Added the support of new part numbers in the STM32G4 Series: STM32G491K(C-E)Ux, STM32G491C(C-E)Ux, STM32G491C(C-E)Tx, STM32G491REYx, STM32G491R(C-E)Tx, STM32G491R(C-E)Ix, STM32G491M(C-E)Sx, STM32G491M(C-E)Tx, STM3...