Hi, I use LWIP to establish a connection, We want to change the IP address, how can I update IP? tcpip_init( NULL, NULL );
/* IP addresses initialization without DHCP (IPv4) */
IP4_ADDR(&ipaddr, IP_ADDRESS[0], IP_ADDRESS[1], IP_ADDRESS[2], IP_A...
I build the server to connected. but if i want change the port and built it again, it can't to usehave any advise?void tcp_server_init(void)
{
tpcb = tcp_new();
if (tpcb != NULL)
{
err_t err;
if((Server_port>=9999)||...
Hi, I'm use the STM32F429This is my FREERTOSConfig.h#define configUSE_PREEMPTION 1
#define configSUPPORT_STATIC_ALLOCATION 0
#define configSUPPORT_DYNAMIC_ALLOCATION 1
#define configUSE_IDLE_HOOK ...