STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1570 Views
  • 0 replies
  • 2 kudos

No printf support on STM32H735G-DK

Hi,I'm trying to run some code on the STM32H735G Development Kit.When simply generating a new firmware in CubeMx (v6.1.1), printf doesn't seem to want to work out of the box and the system hangs. I disable FDCAN init and OCTOSPI init and it can at le...

Arno1 by Senior
  • 2005 Views
  • 4 replies
  • 0 kudos

Resolved! CubeMx and configuring ADC channel(s)

Hi Guys,Im struggling in getting a good way to work with cubemx and multi channel ADC. I want to be able to only change the cubemx file whenever there is a hardware change. Currently i cannot do so because in my firmware i am using HAL_ADC_ConfigChan...

Taxara by Associate III
  • 2851 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeMX STM32H7 I2C Custom Timing not so Custom.

In STM32CubeMX (6.1.0) for STM32H7 the I2C parameter settings allow you to enable Custom Timing. However, the Timing parameter still remains disabled and cannot be set. I would expect that for custom timing, the user could change the Timing paramete...

DOsbo by Senior
  • 2827 Views
  • 4 replies
  • 0 kudos

LWIP PolarSSL Working example

The latest edition of Cube 6.1.1 provides config options for PolarSSL. Can anyone provide some info or working example on how to actually use it? Cannot see anything anywhere documenting the process? Thanks

RStep.2 by Associate
  • 1287 Views
  • 1 replies
  • 0 kudos

Resolved! TIM6 and TIM7 not selectable for ADC

Hallo i´m using STM32F107 and i want to choose in STMCubeMX the TIM6 for triggering the adc in specific times for measuring. My Problem is that i can´t select TIM6 for triggering. What i don´t find is why. In the manual and so on is this possibility ...

0693W000007C2VmQAK.png 0693W000007C2UjQAK.png
TSchi.1 by Associate
  • 1878 Views
  • 3 replies
  • 1 kudos